This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

omx mosaic component frameout control



Hi, I recently use openMax to develop a application.the component connection is decode--mosaic--nf--dei--enc. I set the decode and enc frame out is 30, but don't work. the enc frame out is much large then 30. So I see the mosaic out is great then 30, is about 80, how do i solve this problem to get the encode with 30 frame out file?