Hi Guys,
I'm have routed a DDR3 interface with 2 DDR3L (x8) chips. I have selected a single single ended impedance of 60R and a differential impedance of 120R since the On Device Termination of the ram chip supports 60R and not 50R
My PCB manufacturer has come back and stated that he can only manufacture to a +-10% nominal tollerance which is outside the Zo+5 Zo-5 tollerance.
Would I get a result if I changed the nominal impedance to 50 ohms or will the design tollerate a Z0 +-6R. Please note my design includes a VTT termination regulator.