This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Network-address-translation (NAT) support?

Hello All,

I am using RDK 3.50.

I have built the "iptables" tool and set kernel configure as below:

#
# IP: Netfilter Configuration
#
# CONFIG_NF_DEFRAG_IPV4 is not set
# CONFIG_IP_NF_QUEUE is not set
CONFIG_IP_NF_IPTABLES=y
CONFIG_IP_NF_MATCH_ADDRTYPE=y
CONFIG_IP_NF_MATCH_AH=y
CONFIG_IP_NF_MATCH_ECN=y
CONFIG_IP_NF_MATCH_TTL=y
CONFIG_IP_NF_FILTER=y
CONFIG_IP_NF_TARGET_REJECT=y
CONFIG_IP_NF_TARGET_LOG=y
CONFIG_IP_NF_TARGET_ULOG=y
CONFIG_IP_NF_MANGLE=y
CONFIG_IP_NF_TARGET_ECN=y
CONFIG_IP_NF_TARGET_TTL=y
CONFIG_IP_NF_RAW=y
CONFIG_IP_NF_SECURITY=y

CONFIG_NF_NAT=y
CONFIG_NF_NAT_NEEDED=y
CONFIG_IP_NF_TARGET_MASQUERADE=y
CONFIG_IP_NF_TARGET_NETMAP=y
CONFIG_IP_NF_TARGET_REDIRECT=y
CONFIG_NF_NAT_SNMP_BASIC=y
CONFIG_NF_NAT_PROTO_DCCP=y
CONFIG_NF_NAT_PROTO_GRE=y
CONFIG_NF_NAT_PROTO_UDPLITE=y
CONFIG_NF_NAT_PROTO_SCTP=y
CONFIG_NF_NAT_FTP=y
CONFIG_NF_NAT_IRC=y
CONFIG_NF_NAT_TFTP=y
CONFIG_NF_NAT_AMANDA=y
CONFIG_NF_NAT_PPTP=y
CONFIG_NF_NAT_H323=y
CONFIG_NF_NAT_SIP=y

But when I using the iptables to set NAT configuration, it's not work:

$ iptables -t nat -L

    iptables v1.4.16.3: can't initialize iptables table `nat': Table does not exist (do you need to insmod?)
    Perhaps iptables or your kernel needs to be upgraded.

How to modify kernel configuration to support NAT module?

Any help will be appreciate!!

thank you very much!

BR,

Steven