Other Parts Discussed in Thread: AM3505, AM3517, AM3359
I need to determine if patch 1780.0001--MUSB-Fix-for-CDC-Host-issue-when-streaming-more.patch, mentioned in post Logic OMAP L138 EVM : dongle USB to Ethernet not working on USB 2.0 from 2011 applies to the problem that I am having with the g_ether USB gadget on the Linux 2.6.37 from ti-sdk-am3517-evm-05.05.01.00. The problem is this: regardless of the chunk size sent on a TCP/IP socket, the link eventually hangs, and the host Windows 7 PC times out. It is the entire link that hangs, not just the session/socket. Has anyone used this patch on their AM3505 kernel to fix this? Is there any other patch or post that could direct me to a correct resolution, even one not of TI origin?