This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Does C6748 = OMAP-L138 at the silicon level

Other Parts Discussed in Thread: OMAP-L138, OMAPL138

We are currently using the C6748 DSP.  We are seeing weird lockup issues that appear to be HW related.  As an experiment, we are considering populating a few boards with the OMAP-L138 (since they are pin compatible) and see what happens.  However this experiment would be moot if the two parts shared EXACTLY the same silicon for most of the peripherals (I understand the OMAP part has the ARM core that the C6748 doesn't have).  In particular, we are interested if the DDR2 controller is EXACTLY the same between the C6748 and the OMAP-L138.

Thanks, Dean