Other Parts Discussed in Thread: AM1808
Hi,
We are developing and industrial controller based on AM1808, we want to connect 24 Bit RGB TFT LCD to the 16 Bit LCDC port of the AM1808, should we use the LSB or the MSB data bits from the LCD, is the below configuration correct?
NC -> B0 NC -> G0 NC -> R0
NC -> B1 NC -> G1 NC -> R1
NC -> B2 LCD_D5 -> G2 NC -> R2
LCD_D0 -> B3 LCD_D6 -> G3 LCD_D11 -> R3
LCD_D1 -> B4 LCD_D7 -> G4 LCD_D12 -> R4
LCD_D2 -> B5 LCD_D8 -> G5 LCD_D13 -> R5
LCD_D3 -> B6 LCD_D9 -> G6 LCD_D14 -> R6
LCD_D4 -> B7 LCD_D10 -> G7 LCD_D15 -> R7
Thanks.