Other Parts Discussed in Thread: DM385
hi team,
I'm using DM385, to speed up the boot speed, I port the prefetch mode read to uboot. but It didn't work, it's very weird.
Following is what I did.
I do the NAND access by hand and I programmed the NAND base address to 0x08000000,(write 0x48 to 0x50000078, the GPMC_CONFIG7).
Every thing goes well expect it can’t read out data from 0x08000000. I read 0x200 data from NAND, I can see the perfetch_status is 0x400001C0,
That means it take 0x40 data from the device, that’s good, but only thing is when I want read data from 0x08000000, it trigger the data_abort interrupt.
What else should I do to access the 0x08000000? Why arm can’t decode the 0x08000000, it should be re-directed to GPMC IP, is this right?
Following is my code if you have time to review it, Thanks.
{
#define NAND_BASE 0x8000000
unsigned short a;
a = *(volatile unsigned int *) (0x50000050);
printf("nandcfg %08x cache enabled\n",a);
// send out READ0 command
*(volatile unsigned char *)(0x5000007c) = 0;
*(volatile unsigned char *)(0x50000080) = 0;
*(volatile unsigned char *)(0x50000080) = 0;
*(volatile unsigned char *)(0x50000080) = 0;
*(volatile unsigned char *)(0x50000080) = 0;
*(volatile unsigned char *)(0x50000080) = 0;
*(volatile unsigned char *)(0x5000007c) = 0x30;
udelay(2000000);
// enable ECC
*(volatile unsigned int *) (0x500001f8) = 0x01;
*(volatile unsigned int *) (0x500001fc) = 0x81a000;
*(volatile unsigned int *) (0x500001f4) = 0x11181;
*(volatile unsigned int *) (0x500001f8) = 0x101;
//send out RNDOUT command
*(volatile unsigned char *)(0x5000007c) = 5;
*(volatile unsigned char *)(0x50000080) = 0;
*(volatile unsigned char *)(0x50000080) = 0;
*(volatile unsigned char *)(0x50000080) = 0;
*(volatile unsigned char *)(0x50000080) = 0;
*(volatile unsigned char *)(0x50000080) = 0;
*(volatile unsigned char *)(0x5000007c) = 0xe0;
udelay(2000000);
// config the prefectch register
*(volatile unsigned int *) (0x500001e4) = 0x200;
*(volatile unsigned int *) (0x500001e0) = 0x4080;
*(volatile unsigned int *) (0x500001ec) = 1;
udelay(1000000);
a = *(volatile unsigned int *) (0x500001f0);
printf("stat %08x\n",a);
while(1)
{
a = *(volatile unsigned int *) (0x500001f0);
a = a>> 24;
if(a != 0) break;
}
a = *(volatile unsigned int *) (0x500001f0);
printf("stat %08x\n",a);
a = *(volatile unsigned short *)(NAND_BASE);
printf(" %04x",a);
a = *(volatile unsigned short *)(NAND_BASE);
printf(" %04x",a);
a = *(volatile unsigned short *)(NAND_BASE);
printf(" %04x",a);
a = *(volatile unsigned short *)(NAND_BASE);
printf(" %04x\n",a);
while(1);
}