This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ti8148 GPIO frequency problem

Hi, all:

recently, I was testing the GPIO in TI8148, I would like to use the GPIO to output data in the rate about 500khz, but I follow the user guide of GPIO, found out  that the GPIO data rate is only about 100hz. my test code is run in application program as following :

……

while(1){

system("echo 1 > /sys/class/gpio/gpio48/value");

system("echo 0 > /sys/class/gpio/gpio48/value");

}

……

Then, I test the output rate using oscilloscope  is  about 100 Hz only. I am confised. What is the highest  data rate of the GPIO in TI8148? Are there any other way to Use GPIO in higher data rate?

BR,

qiuxicj