Hi sir,
We have a design that C6678 is connected to BCM56334 through SGMII interface.
BCM56334 is an ethernet Lan Switch. The SGMII interface cannot link up with BCM56334, however.
I see that in document SPRUGV9A that it describes the SGMII Mode of register MR_ADV_ABILITY.
I can not see any description of 1000BASE-X configuration.
I am not sure what is the reson of issure of not linking up? Should C6678 serdes be configured as 1000BASE-X mode?
Thank you very much.