This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Getting Started with C6713 and CCS

Hello Community,

I have been going through tutorials with my C6713 and CCS v3.1 since that is what can with the starter kit. However, I have 5.x license given to me through TI univ. and was wondering if I should upgrade to the newer software. If I should, how do I go about doing this? My goal is to receive signals from the THS1206EVM through the 5-6k Interface board at a freq of around 1MHz. Eventually I plan to generate signals and output through a DAC but for now I would like to focus on the receive channel. Any information regarding this would be greatly appreciated.

Thank you,

Brady