This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

capture performance issue

Hi,

I am working on rdk3.0, I run capture and encode in my application, I find the total encode number is not equal among each channel after long time test.

I press i and see the total fields of capture driver is difference among channels, it will effect encode fps performance. We can't loss any one frame record in my system.

Any reason cause this issue happen?

Thanks,

Jacson

 DEMO:  0: Detected video at CH [0,0] (720x240@59Hz, 1)!!!
 DEMO:  1: Detected video at CH [0,1] (720x240@59Hz, 1)!!!
 DEMO:  2: Detected video at CH [0,2] (720x240@59Hz, 1)!!!
 DEMO:  3: Detected video at CH [0,3] (720x240@59Hz, 1)!!!
 DEMO:  4: Detected video at CH [1,0] (720x240@59Hz, 1)!!!
 DEMO:  5: Detected video at CH [1,1] (720x240@59Hz, 1)!!!
 DEMO:  6: Detected video at CH [1,2] (720x240@59Hz, 1)!!!
 DEMO:  7: Detected video at CH [1,3] (720x240@59Hz, 1)!!!
 DEMO:  8: Detected video at CH [2,0] (720x240@59Hz, 1)!!!
 DEMO:  9: Detected video at CH [2,1] (720x240@59Hz, 1)!!!
 DEMO: 10: Detected video at CH [2,2] (720x240@59Hz, 1)!!!
 DEMO: 11: Detected video at CH [2,3] (720x240@59Hz, 1)!!!
 DEMO: 12: Detected video at CH [3,0] (720x240@59Hz, 1)!!!
 DEMO: 13: Detected video at CH [3,1] (720x240@59Hz, 1)!!!
 DEMO: 14: Detected video at CH [3,2] (720x240@59Hz, 1)!!!
 DEMO: 15: Detected video at CH [3,3] (720x240@59Hz, 1)!!!
 
 [m3vpss ]  
 [m3vpss ]  *** Capture Driver Advanced Statistics ***
 [m3vpss ]  
 [m3vpss ]  VIP Parser Reset Count : 0
 [m3vpss ]  
 [m3vpss ]      |   Total    Even     Odd  Total  Even   Odd  Min /  Max  Min /  Max Dropped Fid Repeat Frame Error Y/C
 [m3vpss ]  CH  |  Fields  Fields  Fields    FPS   FPS   FPS       Width      Height  Fields      Count (Desc Error Y/C)
 [m3vpss ]  ------------------------------------------------------------------------------------------------------------
 [m3vpss ]  000 | 3094035 1547018 1547017     59    29    29  720 /  720  243 /  244       1          1 0/0 (0/0)
 [m3vpss ]  001 | 3094043 1547022 1547021     59    29    29  720 /  720  243 /  244       1          0 0/0 (0/0)
 [m3vpss ]  002 | 3094043 1547022 1547021     59    29    29  720 /  720  243 /  244       1          0 0/0 (0/0)
 [m3vpss ]  003 | 3094145 1547073 1547072     59    29    29  720 /  720  243 /  244       1          1 0/0 (0/0)
 [m3vpss ]  100 | 3093995 1546998 1546997     59    29    29  720 /  720  243 /  244       1          1 0/0 (0/0)
 [m3vpss ]  101 | 3093995 1546998 1546997     59    29    29  720 /  720  243 /  244       1          1 0/0 (0/0)
 [m3vpss ]  102 | 3094042 1547022 1547020     59    29    29  720 /  720  243 /  244       1          1 0/0 (0/0)
 [m3vpss ]  103 | 3094043 1547022 1547021     59    29    29  720 /  720  243 /  244       1          0 0/0 (0/0)
 [m3vpss ]  200 | 3093994 1546997 1546997     59    29    29  720 /  720  243 /  244       1          0 0/0 (0/0)
 [m3vpss ]  201 | 3093994 1546997 1546997     59    29    29  720 /  720  243 /  244       1          0 0/0 (0/0)
 [m3vpss ]  202 | 3093994 1546997 1546997     59    29    29  720 /  720  243 /  244       1          0 0/0 (0/0)
 [m3vpss ]  203 | 3093994 1546997 1546997     59    29    29  720 /  720  243 /  244       1          0 0/0 (0/0)
 [m3vpss ]  300 | 3093994 1546997 1546997     59    29    29  720 /  720  243 /  244       1          0 0/0 (0/0)
 [m3vpss ]  301 | 3093994 1546997 1546997     59    29    29  720 /  720  243 /  244       1          0 0/0 (0/0)
 [m3vpss ]  302 | 3093994 1546997 1546997     59    29    29  720 /  720  243 /  244       1          0 0/0 (0/0)
 [m3vpss ]  303 | 3093994 1546997 1546997     59    29    29  720 /  720  243 /  244       1          0 0/0 (0/0)
 [m3vpss ]  
 [m3vpss ]  VIP Capture Port 0 | DescMissMatch1 = 0, DescMissMatch2 = 0 , DescMissMatch3 = 0
 [m3vpss ]  VIP Capture Port 1 | DescMissMatch1 = 0, DescMissMatch2 = 0 , DescMissMatch3 = 0
 [m3vpss ]  VIP Capture Port 2 | DescMissMatch1 = 0, DescMissMatch2 = 0 , DescMissMatch3 = 0
 [m3vpss ]  VIP Capture Port 3 | DescMissMatch1 = 0, DescMissMatch2 = 0 , DescMissMatch3 = 0
 [m3vpss ]  
 [m3vpss ]  *** Capture List Manager Advanced Statistics ***
 [m3vpss ]  
 [m3vpss ]  List Post Count        : 24861198
 [m3vpss ]  List Stall Count       : 0
 [m3vpss ]  List Post Time (ms)    : Max = 4, Min = 0, Avg = 0, Total = 375397
 [m3vpss ]  INTC Timeout Count     : (0, 0) (Min timeout value = 898, 972)
 [m3vpss ]  Descriptor miss found count : 0
 [m3vpss ]  
 [m3vpss ]  
 [m3vpss ]  VIP and VPDMA registers,
 [m3vpss ]  VIP0 : FIQ_STATUS  : 0x4810551c = 0x0000d400
 [m3vpss ]  VIP1 : FIQ_STATUS  : 0x48105a1c = 0x0000d400
 [m3vpss ]  VPDMA: LIST_BUSY   : 0x4810d00c = 0x00060000
 [m3vpss ]  
 [m3vpss ]  
 [m3vpss ]  51842257: CAPTURE: Fields = 49504270 (fps = 126, CPU Load = 0)
 [m3vpss ]  51842257: CAPTURE: Num Resets = 0 (Avg 0 ms per reset)
 [m3vpss ]  51842257: SYSTEM  : FREE SPACE : System Heap      = 5744 B, Mbx = 10235 msgs)
 [m3vpss ]  51842257: SYSTEM  : FREE SPACE : SR0 Heap         = 10811648 B (10 MB)
 [m3vpss ]  51842257: SYSTEM  : FREE SPACE : Frame Buffer     = 691413120 B (659 MB)
 [m3vpss ]  51842257: SYSTEM  : FREE SPACE : Bitstream Buffer = 185421952 B (176 MB)
 [m3vpss ]  51842265: SYSTEM  : FREE SPACE : Tiler 8-bit      = 89128960 B (85 MB)  - TILER ON
 [m3vpss ]  51842265: SYSTEM  : FREE SPACE : Tiler 16-bit     = 44040192 B (42 MB)  - TILER ON