This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

omap5432uevm es2.0 Parallel display interface outputs 2560x1600 resolution



omap5432uevm es2.0 how to use 5AJ.1.5 from Parallel display interface outputs 2560x1600 resolution, please help.

  • Maximum output resolution supported is 1920x1200. Please see OMAP5432 product folder for more details. 

  • Hi Gaurav
    Thank you for your response,

    Ask another question.

    Use 5aj.1.5 version, omap5432uevm borad, in the DSS.C file to add the following two lines of code,

    REG_FLD_MOD (DSS_PLL_CONTROL, 0, 16, 16);

    REG_FLD_MOD (DSS_PLL_CONTROL, 0, 17, 17);

    Parallel display port no signal output. Patch files can be used if there is?

    Before using the panda board (omap4460), the file is added in DSS.C

    REG_FLD_MOD (DSS_PLL_CONTROL, 1, 17, 17);

    HDMI resolution can be made ​​in parallel port output samples with Timing.