When i boot from SD card i have 3 options to run my WinCE:
(1) LAN
(2) USB RNDIS
(3) nk.bin file on SD-card
The first (LAN) is the default.
What should i change in eboot sources if i want the third option to be the default ???
(Microsoft Windows CE Bootloader Common Library Version 1.4 Built Jun 18 2013 14:24:36
Texas Instruments Windows CE EBOOT for Mistral OMAP EVM, Built Jun 18 2013 at 14:27:41
EBOOT Version 1.1, BSP 6.15.00)