This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Boot time and later messages from jss2

Other Parts Discussed in Thread: AM3517, AM3505

I will eventually need to show the cause of or eliminate the following:

[    8.416046] CLEANMARKER node found at 0x00d90000 has totlen 0xc != normal 0x0
[    8.427612] CLEANMARKER node found at 0x00da0000 has totlen 0xc != normal 0x0
[    8.481536] Empty flash at 0x00dafffc ends at 0x00db0000
[    8.487121] CLEANMARKER node found at 0x00db0000 has totlen 0xc != normal 0x0
[    8.700805] Empty flash at 0x01c5988c ends at 0x01c5a000

I get a plethora of the above when booting from my 8-bit Micron NAND flash drive, as the kernel tries to bring up the root file system.  It is successful, but I would like to know if these messages indicate a problem.  If so, what problem?  Thanks.

[  276.035980] JFFS2 notice: (682) check_node_data: wrong data CRC in data node at 0x051b720c: read 0x2de5fbbc, calculated 0xcd8f5697.

The above shows up intermittently while the system is running after boot.  The same questions apply.\

I am running a modified AM3517 EVM linux kernel on an AM3505.