This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Endpoint-to-Endpoint communications using PCIe switch

Hi all,

Working on DSP C6678 communications using PCIe switch, i can perform DSP-to-DSP memory transfer (one as RC and other as EP).

OK, now i’m trying to add a third DSP, so one DSP is configured as RC and the two others are configured as EP.

The main objective is to verify EP-to-EP communications using PCIe switch.

May i ask: It is possible to communicate directly two EPs without RC intervention? if not, there there are some things that I should keep in mind in this case?

I need more explanations please?