Must the CDR field in SGMII RX Configuration Register (SGMII_SERDES_CGFRXn) be always set to 000b?
Best regards,
Daisuke
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Must the CDR field in SGMII RX Configuration Register (SGMII_SERDES_CGFRXn) be always set to 000b?
Best regards,
Daisuke
Daisuke,
From Table 3-136, SPRUGV9B: Gigabit Ethernet (GbE) Switch Subsystem
17-15 CDR Clock/data recovery. Configures the clock recovery algorithm.
000 = First order, threshold of 1. Phase offset tracking up to ±488ppm. Suitable for use in asynchronous systems with low
frequency offset.
001 = First order, threshold of 17. Phase offset tracking up to ±325ppm. Suitable for use in synchronous systems. Offers
superior rejection of random jitter, but is less responsive to systematic variation such as sinusoidal jitter.
010-111 = Reserved
Regards, Eric
Hi Eric,
Thank you for your reply.
Our customer is simulating for SGMII and SRIO with the AMI models.
They want to configure the SerDes Registers according to the IBIS AMI parameters.
However those details cannot be found. The SGMII specifications seem not to be public.
Therefore it is necessary to get the SGMII clock recovery algorithm details here.
Any advice or information you could provide would be greatly appreciated.
Best regards,
Daisuke