Other Parts Discussed in Thread: OMAP-L138
Hello all,
I am using Logic PD's Evmomapl138, Code Composer Studio v5 and the StarterWare libraries.
I used the StarterWare example spiflash to understand how to manage the data transmission thru the SPI using interrupts. Right now, I have a buffer that has the data stored and in the interrupt code I have a while loop where I put the data in the SPIDAT1 register where I understand, could be wrong, that the data that will be transmitted is sent.
Code in interrupt below:
if (intCode == SPI_TX_BUF_EMPTY){
len--;
SPITransmitData1(SOC_SPI_1_REGS, *tx_buff_ptr);
tx_buff_ptr++;
if (!len){
SPIIntDisable(SOC_SPI_1_REGS, SPI_TRANSMIT_INT);
}
}
Is there anyway I can phisically see the output of the data, for example, where the data is being output, (serial interface, for example? ) so I can see the data that I see in the register?
Any ideas, suggestions are greatly appreciated.
Thanks,
Michelle