I am currently chasing a memory corruption error and am having trouble understanding the errors in my raw log file.
I am using a custom board with an OMAP L138, Linux on the ARM and DSP/BIOS 5.41.13 on the DSP. I am using CCSv5 Compiler 7.3.4
The raw logs show the following errors numerous times when I am running -
"PRD begin- <unkown handle> (0x00000000)
Unknown event ID 65535"
These show up several times in the log file prior to my memory corruption.
Sometimes I will also see an SWI - unkown handle.
Please advise,
Thanks,
Joyce