This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

10" Tablet Design Instead Of Just 7"



Can anyone tell me if this design can be modified to build a 10" screen instead of a 7" screen? Or is there another design kit for this?

I am working on a project that could require several thousand 10" tablets with aluminum casings and Android for the operating system...I would also like to increase the memory as our application will be native to the tablet as well, and is fairly large....

Thank you in advance for your help :-)

JR