Hi
I'm trying building ubl for AM1808.
However, it dosn't work well.
I'm very happy if somebody give me advices to make it well.
<our process>
1.CCS Project
First, I found dvsdk_omapl138-evm_4_01_00_09_setuplinux, and executed it on Linux.
Then, I extracted following to Windows.
\psp\board-utilities\src\boot-strap\armubl-03.20.00.14\ccsv3.3\ubl-omapl1x8.pjt
Next, on IDE, I imported above project.
File->Import -> Code Composer Studio -> Legacy CCSv3.3 Projects
2.IDE
Code Composer Studio Version: 5.4.0.00091 on Windows7
3.SoC
Our target board has AM1808
4.Writing tool
sfh_OMAP-L138.exe which is included in OMAP-L138_FlashAndBootUtils_2_40
5.Modified
I changed tool hex470.exe to armhex.exe.
The hex470 was not included in CCS 5.4.
I could build successfully, however, it dosn't work on our target board.
The prebuild ubl works well which is included following.
\psp\board-utilities\images\boot-strap\arm-nand-ais.bin