This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reading Data ID of a received CSI2 image data packet

Hi,

I am working with a custom OMAP4470 board.

I have connected a HDMI input to CSI2 bridge to CSI2A port of OMAP.

The HDMI-CSI2 bridge is configured to give 1080i interlaced video to OMAP.

The HDMI-CSI2 bridge outputs top and bottom field video with different data ID in CSI packets.

I need to read this field  information(data ID) transmitted with CSI2 image data packets.

Is there a way to read the data ID of CSI image data packets received at OMAP ?

Regards,

Sanjeev R