Other Parts Discussed in Thread: TVP5158
hi,
i am using dm8168 , dvrrdk 3.0. and i use demo vcap_vdis . but videoDecoderDriver is not tvp5158,.and use ourselves.
i set parameters as follows: and use 2 vip instances ,vip0 port a, vip1 porta . .. and each vip is configured to 16bits
if(vipInstId == 0)
{
pCaptureInstPrm->vipInstId = SYSTEM_CAPTURE_INST_VIP0_PORTA;
pCaptureInstPrm->videoDecoderId = SYSTEM_DEVICE_VID_DEC_ADV7441A_HDMI_DRV;//null value
pCaptureInstPrm->standard = SYSTEM_STD_720P_60;
}
else if(vipInstId == 1)
{
pCaptureInstPrm->vipInstId = SYSTEM_CAPTURE_INST_VIP1_PORTA;
pCaptureInstPrm->videoDecoderId = SYSTEM_DEVICE_VID_DEC_ADV7441A_HDMI_DRV;//null value
pCaptureInstPrm->standard = SYSTEM_STD_720P_60;
}
DVR_NETRA Board (Monday, 11 April 2011) login: root root@dm816x:~# busybox mount -t nfs -o nolock 192.168.9.157:/boardnfs/ /home/libin/ root@dm816x:~# cd /home/libin/libin/ti816x/ root@dm816x:/home/libin/libin/ti816x# ls 16bits.out firmware load.sh run_link_api.sh bin init.sh onlyVip0PortA.out scripts demoTest.out kermod onlyVip1PortA.out ti816x.tar.gz demo_ini libin.sh open_bin unload.sh dvr_rdk_demo_mcfw_api_fb.out libin.sh_16 run.sh validate.sh env.sh libin.sh_8 run_gui.sh xux_bk root@dm816x:/home/libin/libin/ti816x# ./init.sh *** Bootargs Validated for mem param *** *** Bootargs Validated for notifyk.vpssm3 params *** Kernel bootargs validated numid=1,iface=MIXER,name='PCM Playback Volume' ; type=INTEGER,access=rw---R--,values=2,min=0,max=127,step=0 : values=127,127 | dBscale-min=-63.50dB,step=0.50dB,mute=0 [c6xdsp ] Remote Debug Shared Memory @ 0xbf000000 [m3video] Remote Debug Shared Memory @ 0xbf005020 [m3vpss ] Remote Debug Shared Memory @ 0xbf00a040 Setting DMM priority for [DUCATI ] to [0] ( 0x4e000624 = 0x08000000 ) Setting DMM priority for [HDVICP0 ] to [2] ( 0x4e000634 = 0x0000000a ) Setting DMM priority for [HDVICP1 ] to [2] ( 0x4e000634 = 0x000a0000 ) Setting DMM priority for [HDVICP2 ] to [2] ( 0x4e000634 = 0x00a00000 ) /home/libin/libin/ti816x root@dm816x:/home/libin/libin/ti816x# ./load.sh Attached to slave procId 2. Loaded file ../firmware/dvr_rdk_fw_m3vpss.xem3 on slave procId 2. Started slave procId 2. After Ipc_loadcallback status [0x00000000] [m3vpss ] ***** SYSTEM : Frequency <ORG> - 250000000, <NEW> - 280000000 [m3vpss ] notify_attach rtnVal 0 [m3vpss ] initProxyServer rtnVal 0 [m3vpss ] [m3vpss ] *** UTILS: CPU KHz = 560000 Khz *** [m3vpss ] [m3vpss ] 43: SYSTEM : System Common Init in progress !!! [m3vpss ] 43: SYSTEM: IPC init in progress !!! [m3vpss ] 43: SYSTEM: Attaching to [HOST] ... [m3vpss ] 1043: SYSTEM: Attaching to [HOST] ... [m3vpss ] 1045: SYSTEM: Attaching to [HOST] ... SUCCESS !!! [m3vpss ] 1045: SYSTEM: Attaching to [DSP] ... After Ipc_startcallback status [0x097d2000] Attached to slave procId 1. Loaded file ../firmware/dvr_rdk_fw_m3video.xem3 on slave procId 1. Started slave procId 1. After Ipc_loadcallback status [0x00000000] [m3video] ***** SYSTEM : Frequency <ORG> - 250000000, <NEW> - 280000000 [m3vpss ] 2045: SYSTEM: Attaching to [DSP] ... [m3video] [m3video] *** UTILS: CPU KHz = 560000 Khz *** [m3video] [m3video] 1594: SYSTEM : System Common Init in progress !!! [m3video] 1594: SYSTEM: IPC init in progress !!! [m3video] 1594: SYSTEM: Attaching to [HOST] ... [m3video] 2594: SYSTEM: Attaching to [HOST] ... [m3video] 2596: SYSTEM: Attaching to [HOST] ... SUCCESS !!! [m3video] 2596: SYSTEM: Attaching to [DSP] ... After Ipc_startcallback status [0x00000000] Attached to slave procId 0. Loaded file ../firmware/dvr_rdk_fw_c6xdsp.xe674 on slave procId 0. Started slave procId 0. After Ipc_loadcallback status [0x00000000] After Ipc_startcallback status [0x00000000] [c6xdsp ] ***** SYSTEM : Frequency <ORG> - 800000000, <NEW> - 800000000 [m3video] 3596: SYSTEM: Attaching to [DSP] ... [m3vpss ] 3045: SYSTEM: Attaching to [DSP] ... [c6xdsp ] [c6xdsp ] *** UTILS: CPU KHz = 800000 Khz *** [c6xdsp ] [c6xdsp ] 5: SYSTEM : System Common Init in progress !!! [c6xdsp ] 5: SYSTEM: IPC init in progress !!! [c6xdsp ] 5: SYSTEM: Attaching to [HOST] ... [c6xdsp ] 1029: SYSTEM: Attaching to [HOST] ... [c6xdsp ] 1031: SYSTEM: Attaching to [HOST] ... SUCCESS !!! [c6xdsp ] 1031: SYSTEM: Attaching to [VIDEO-M3] ... [m3vpss ] 4045: SYSTEM: Attaching to [DSP] ... [c6xdsp ] Remote Debug Shared Memory @ 0xbf000000 [m3video] Remote Debug Shared Memory @ 0xbf005020 [m3vpss ] Remote Debug Shared Memory @ 0xbf00a040 [m3video] 4596: SYSTEM: Attaching to [DSP] ... [c6xdsp ] 2055: SYSTEM: Attaching to [VIDEO-M3] ... [m3vpss ] 5045: SYSTEM: Attaching to [DSP] ... [c6xdsp ] 2796: SYSTEM: Attaching to [VIDEO-M3] ... SUCCESS !!! [m3video] 5596: SYSTEM: Attaching to [DSP] ... [c6xdsp ] 2796: SYSTEM: Attaching to [VPSS-M3] ... [m3video] 5596: SYSTEM: Attaching to [DSP] ... SUCCESS !!! [m3video] 5596: SYSTEM: Attaching to [VPSS-M3] ... [m3vpss ] 6045: SYSTEM: Attaching to [DSP] ... [m3video] 6596: SYSTEM: Attaching to [VPSS-M3] ... [c6xdsp ] 3819: SYSTEM: Attaching to [VPSS-M3] ... [c6xdsp ] 4269: SYSTEM: Attaching to [VPSS-M3] ... SUCCESS !!! [m3vpss ] 7045: SYSTEM: Attaching to [DSP] ... [c6xdsp ] 4269: SYSTEM: Opening MsgQ Heap [IPC_MSGQ_MSG_HEAP] ... [m3vpss ] 7045: SYSTEM: Attaching to [DSP] ... SUCCESS !!! [m3vpss ] 7045: SYSTEM: Attaching to [VIDEO-M3] ... [m3video] 7596: SYSTEM: Attaching to [VPSS-M3] ... [m3vpss ] 8045: SYSTEM: Attaching to [VIDEO-M3] ... [c6xdsp ] 5294: SYSTEM: Opening MsgQ Heap [IPC_MSGQ_MSG_HEAP] ... [m3video] 8045: SYSTEM: Attaching to [VPSS-M3] ... SUCCESS !!! [m3vpss ] 8045: SYSTEM: Attaching to [VIDEO-M3] ... SUCCESS !!! [c6xdsp ] 5294: SYSTEM: Creating MsgQ [DSP_MSGQ] ... [m3video] 8045: SYSTEM: Opening MsgQ Heap [IPC_MSGQ_MSG_HEAP] ... [m3vpss ] 8045: SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP] ... [c6xdsp ] 5294: SYSTEM: Creating MsgQ [DSP_ACK_MSGQ] ... [m3video] 8046: SYSTEM: Creating MsgQ [VIDEO-M3_MSGQ] ... [m3vpss ] 8046: SYSTEM: Creating MsgQ [VPSS-M3_MSGQ] ... [c6xdsp ] 5294: SYSTEM: Notify register to [HOST] line 0, event 15 ... [m3video] 8046: SYSTEM: Creating MsgQ [VIDEO-M3_ACK_MSGQ] ... [m3vpss ] 8046: SYSTEM: Creating MsgQ [VPSS-M3_ACK_MSGQ] ... [c6xdsp ] 5294: SYSTEM: Notify register to [VIDEO-M3] line 0, event 15 ... [m3video] 8048: SYSTEM: Notify register to [HOST] line 0, event 15 ... [m3vpss ] 8047: SYSTEM: Notify register to [HOST] line 0, event 15 ... [c6xdsp ] 5294: SYSTEM: Notify register to [VPSS-M3] line 0, event 15 ... [m3video] 8048: SYSTEM: Notify register to [DSP] line 0, event 15 ... [m3vpss ] 8048: SYSTEM: Notify register to [DSP] line 0, event 15 ... [c6xdsp ] 5294: SYSTEM: IPC init DONE !!! [m3video] 8048: SYSTEM: Notify register to [VPSS-M3] line 0, event 15 ... [m3vpss ] 8048: SYSTEM: Notify register to [VIDEO-M3] line 0, event 15 ... [m3video] 8048: SYSTEM: IPC init DONE !!! [m3vpss ] 8048: SYSTEM: IPC init DONE !!! [m3video] 8055: MEM: Shared Region 2: Base = 0xb0000000, Length = 0x0e9c0000 (233 MB) [m3vpss ] 8054: MEM: Shared Region 2: Base = 0xb0000000, Length = 0x0e9c0000 (233 MB) [m3video] 8055: MEM: Shared Region 1: Base = 0x88000000, Length = 0x15080000 (336 MB) [m3vpss ] 8055: MEM: Shared Region 1: Base = 0x88000000, Length = 0x15080000 (336 MB) [c6xdsp ] 5296: MEM: Shared Region 2: Base = 0xb0000000, Length = 0x0e9c0000 (233 MB) [m3video] 8057: SYSTEM : System Common Init Done !!! [m3vpss ] 8056: SYSTEM : System Common Init Done !!! [c6xdsp ] 5296: MEM: Shared Region 1: Base = 0x88000000, Length = 0x15080000 (336 MB) [m3video] 8057: SYSTEM : System Video Init in progress !!! [m3vpss ] 8056: SYSTEM : System VPSS Init in progress !!! [c6xdsp ] 5297: SYSTEM : System Common Init Done !!! [m3video] 8057: SYSTEM : System Video Init Done !!! [m3vpss ] 8056: SYSTEM: VPDMA is Busy (0x00040000) !!! [c6xdsp ] 5169: SYSTEM : System DSP Init in progress !!! [m3video] 8057: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_0] in region 0 ... [c6xdsp ] 5169: SYSTEM : RpeServer_init() done... Ret Val 0!!! [m3video] 8057: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_0] in region 0 ... [c6xdsp ] 5300: SYSTEM: Creating ListMP [DSP_IPC_OUT_19] in region 0 ... [m3video] 8058: SYSTEM: ListElem Shared Addr = 0xbf18b680 [c6xdsp ] 5301: SYSTEM: Creating ListMP [DSP_IPC_IN_19] in region 0 ... [m3video] 8059: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_1] in region 0 ... [c6xdsp ] 5301: SYSTEM: ListElem Shared Addr = 0xbf192080 [m3video] 8060: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_1] in region 0 ... [c6xdsp ] 5302: SYSTEM: Creating ListMP [DSP_IPC_OUT_20] in region 0 ... [m3video] 8060: SYSTEM: ListElem Shared Addr = 0xbf18eb80 [c6xdsp ] 5302: SYSTEM: Creating ListMP [DSP_IPC_IN_20] in region 0 ... [m3video] 8065: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_19] in region 0 ... [c6xdsp ] 5302: SYSTEM: ListElem Shared Addr = 0xbf1b1a80 [m3video] 8065: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_19] in region 0 ... [c6xdsp ] 5303: SYSTEM: Creating ListMP [DSP_IPC_OUT_21] in region 0 ... [m3video] 8065: SYSTEM: ListElem Shared Addr = 0xbf22c480 [c6xdsp ] 5303: SYSTEM: Creating ListMP [DSP_IPC_IN_21] in region 0 ... [c6xdsp ] 5303: SYSTEM: ListElem Shared Addr = 0xbf1d1480 [c6xdsp ] 5304: SYSTEM: Creating ListMP [DSP_IPC_OUT_24] in region 0 ... [c6xdsp ] 5304: SYSTEM: Creating ListMP [DSP_IPC_IN_24] in region 0 ... [c6xdsp ] 5304: SYSTEM: ListElem Shared Addr = 0xbf1f0e80 [c6xdsp ] 5305: SYSTEM: Creating ListMP [DSP_IPC_OUT_25] in region 0 ... [c6xdsp ] 5305: SYSTEM: Creating ListMP [DSP_IPC_IN_25] in region 0 ... [c6xdsp ] 5305: SYSTEM: ListElem Shared Addr = 0xbf20e980 [c6xdsp ] !!WARNING.Resource already registered:2 [c6xdsp ] 5177: SYSTEM : Initializing Links !!! [c6xdsp ] 5305: SYSTEM : FREE SPACE : System Heap = 10268448 B, Mbx = 10240 msgs) [m3video] 8067: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_20] in region 0 ... [m3video] 8067: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_20] in region 0 ... [c6xdsp ] 5188: SYSTEM : Initializing Links ... DONE !!! [m3video] 8067: SYSTEM: ListElem Shared Addr = 0xbf24be80 [m3video] 8069: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_21] in region 0 ... [c6xdsp ] 5188: SYSTEM : System DSP Init Done !!! [m3video] 8070: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_21] in region 0 ... [m3video] 8070: SYSTEM: ListElem Shared Addr = 0xbf26b880 [m3video] 8080: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_24] in region 0 ... [m3video] 8080: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_24] in region 0 ... [m3video] 8080: SYSTEM: ListElem Shared Addr = 0xbf28b280 [m3video] 8082: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_25] in region 0 ... [m3video] 8082: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_25] in region 0 ... [m3video] 8083: SYSTEM: ListElem Shared Addr = 0xbf2a8d80 [m3video] 8084: HDVICP: Doing PRCM for IVAHD[0] ... [m3video] 8084: HDVICP: PRCM for IVAHD[0] ... DONE. [m3video] 8084: HDVICP: Doing PRCM for IVAHD[1] ... [m3video] 8084: HDVICP: PRCM for IVAHD[1] ... DONE. [m3video] 8085: HDVICP: Doing PRCM for IVAHD[2] ... [m3video] 8085: HDVICP: PRCM for IVAHD[2] ... DONE. [m3video] 8085: SYSTEM : Initializing Links !!! [m3video] 8085: SYSTEM : FREE SPACE : System Heap = 6280232 B, Mbx = 10240 msgs) [m3video] 8085: SYSTEM : FREE SPACE : SR0 Heap = 13868416 B (13 MB) [m3video] 8085: SYSTEM : FREE SPACE : Frame Buffer = 245104512 B (233 MB) [m3video] 8086: SYSTEM : FREE SPACE : Bitstream Buffer = 352845696 B (336 MB) [m3video] 8086: SYSTEM: Opening MsgQ [VPSS-M3_MSGQ] ... [m3video] 8086: SYSTEM : FREE SPACE : Tiler 8-bit = 134217728 B (128 MB) - TILER ON [m3video] 8087: SYSTEM : FREE SPACE : Tiler 16-bit = 134217728 B (128 MB) - TILER ON [m3video] 8108: SYSTEM : Initializing Links ... DONE !!! [m3vpss ] 9056: SYSTEM: VPDMA is Busy (0x00040000) !!! [m3vpss ] 10056: SYSTEM: VPDMA is Busy (0x00040000) !!! [m3vpss ] 11056: SYSTEM: VPDMA is Busy (0x00040000) !!! [m3vpss ] 12056: SYSTEM: VPDMA is Busy (0x00040000) !!! [m3vpss ] 13056: SYSTEM: VPDMA is Busy (0x00040000) !!! [m3vpss ] 14056: SYSTEM: VPDMA is Busy (0x00040000) !!! [m3vpss ] 15056: SYSTEM: VPDMA is Busy (0x00040000) !!! [m3vpss ] 16056: SYSTEM: VPDMA is Busy (0x00040000) !!! [m3vpss ] 17056: SYSTEM: VPDMA is Busy (0x00040000) !!! [m3vpss ] 18056: SYSTEM: VPDMA is Busy (0x00040000) !!! [m3vpss ] 19056: SYSTEM: VPDMA is Busy (0x00040000) !!! [m3vpss ] 20056: SYSTEM: VPDMA is Busy (0x00040000) !!! [m3vpss ] 21056: SYSTEM: VPDMA is Busy (0x00040000) !!! [m3vpss ] 22056: SYSTEM: VPDMA is Busy (0x00040000) !!! [m3vpss ] 23056: SYSTEM: VPDMA is Busy (0x00040000) !!! [m3vpss ] 24056: SYSTEM: VPDMA is Busy (0x00040000) !!! [m3vpss ] 25056: SYSTEM: VPDMA is Busy (0x00040000) !!! [m3vpss ] 26056: SYSTEM: VPDMA is Busy (0x00040000) !!! [m3vpss ] 27056: SYSTEM: VPDMA is Busy (0x00040000) !!! [m3vpss ] 28056: SYSTEM: All VPDMA Free !!! [m3vpss ] === HDVPSS Clocks are enabled === [m3vpss ] === HDVPSS is fully functional === [m3vpss ] === HDVPSS module is not in standby === [m3vpss ] === I2C1 Clk is active === [m3vpss ] PLATFORM: UNKNOWN CPU detected, defaulting to VPS_PLATFORM_CPU_REV_2_0 [m3vpss ] 28061: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_0] in region 0 ... [m3vpss ] 28062: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_0] in region 0 ... [m3vpss ] 28062: SYSTEM: ListElem Shared Addr = 0xbf2c6880 [m3vpss ] 28064: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_1] in region 0 ... [m3vpss ] 28064: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_1] in region 0 ... [m3vpss ] 28064: SYSTEM: ListElem Shared Addr = 0xbf2c9d80 [m3vpss ] 28074: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_19] in region 0 ... [m3vpss ] 28074: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_19] in region 0 ... [m3vpss ] 28075: SYSTEM: ListElem Shared Addr = 0xbf2cd280 [m3vpss ] 28077: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_20] in region 0 ... [m3vpss ] 28077: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_20] in region 0 ... [m3vpss ] 28077: SYSTEM: ListElem Shared Addr = 0xbf2ecc80 [m3vpss ] 28079: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_21] in region 0 ... [m3vpss ] 28079: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_21] in region 0 ... [m3vpss ] 28079: SYSTEM: ListElem Shared Addr = 0xbf30c680 [m3vpss ] 28081: SYSTEM : HDVPSS Drivers Version: HDVPSS_01_00_01_37 [m3vpss ] 28081: SYSTEM : FVID2 Init in progress !!! [m3vpss ] 28136: SYSTEM : FVID2 Init in progress DONE !!! [m3vpss ] 28136: SYSTEM : Device Init in progress !!! [m3vpss ] initPrms.isI2cInitReq = 0 [m3vpss ] initPrms.isI2cInitReq = 0 [m3vpss ] 28140: SYSTEM : Device Init in progress DONE !!! [m3vpss ] 28258: SYSTEM : System VPSS Init Done !!! [m3vpss ] 28258: UTILS: DMA: HWI Create for INT63 !!! [m3vpss ] 28258: SYSTEM : Initializing Links !!! [m3vpss ] 28259: SYSTEM : FREE SPACE : System Heap = 13024 B, Mbx = 10240 msgs) [m3vpss ] 28259: SYSTEM : FREE SPACE : SR0 Heap = 13452672 B (12 MB) [m3vpss ] 28259: SYSTEM : FREE SPACE : Frame Buffer = 240794496 B (229 MB) [m3vpss ] 28259: SYSTEM : FREE SPACE : Bitstream Buffer = 352845696 B (336 MB) [m3vpss ] 28259: SYSTEM : FREE SPACE : Tiler 8-bit = 134217728 B (128 MB) - TILER ON [m3vpss ] 28259: SYSTEM : FREE SPACE : Tiler 16-bit = 134217728 B (128 MB) - TILER ON [m3vpss ] Received character 's' [m3vpss ] 28341: SYSTEM : Initializing Links ... DONE !!! [c6xdsp ] Remote Debug Shared Memory @ 0xbf000000 [m3video] Remote Debug Shared Memory @ 0xbf005020 [m3vpss ] Remote Debug Shared Memory @ 0xbf00a040 [m3video] Received character 's' [m3vpss ] 28341: SYSTEM : Set Static L3 pressure for HDVPSS as High [c6xdsp ] Remote Debug Shared Memory @ 0xbf000000 [m3video] Remote Debug Shared Memory @ 0xbf005020 [m3vpss ] Remote Debug Shared Memory @ 0xbf00a040 [c6xdsp ] Received character 's' /home/libin/libin/ti816x ORG 0x46c00524: 0 NEW 0x46c00524: 2 root@dm816x:/home/libin/libin/ti816x# ./demoTest.out ========= Main Menu ========= 1: VCAP + VENC + VDEC + VDIS - Progressive SD Encode + Decode 2: VCAP + VENC + VDIS - SD Encode ONLY 3: VCAP + VENC + VDIS - HD Encode ONLY 4: VDEC + VDIS - SD/HD Decode ONLY 5: VCAP + VDIS - NO Encode or Decode e: Exit Enter Choice: 5 --------------- CHANNEL DETAILS------------- Capture Channels => 16 Disp Channels => 16 ------------------------------------------- 0: SYSTEM: System Common Init in progress !!! 0: SYSTEM: IPC init in progress !!! 17: SYSTEM: Opening MsgQ Heap [IPC_MSGQ_MSG_HEAP] ... 19: SYSTEM: Creating MsgQ [HOST_MSGQ] ... 21: SYSTEM: Creating MsgQ [HOST_ACK_MSGQ] ... 23: SYSTEM: Opening MsgQ [DSP_MSGQ] ... 23: SYSTEM: Opening MsgQ [VIDEO-M3_MSGQ] ... 24: SYSTEM: Opening MsgQ [VPSS-M3_MSGQ] ... 25: SYSTEM: Notify register to [DSP] line 0, event 15 ... 25: SYSTEM: Notify register to [VIDEO-M3] line 0, event 15 ... 25: SYSTEM: Notify register to [VPSS-M3] line 0, event 15 ... 26: SYSTEM: IPC init DONE !!! 27: SYSTEM: Creating ListMP [HOST_IPC_OUT_24] in region 0 ... 29: SYSTEM: Creating ListMP [HOST_IPC_IN_24] in region 0 ... 31: SYSTEM: ListElem Shared Addr = 0x2b13f080 32: SYSTEM: Creating ListMP [HOST_IPC_OUT_25] in region 0 ... 34: SYSTEM: Creating ListMP [HOST_IPC_IN_25] in region 0 ... 35: SYSTEM: ListElem Shared Addr = 0x2b15cb80 37: SYSTEM: Creating ListMP [HOST_IPC_OUT_19] in region 0 ... 39: SYSTEM: Creating ListMP [HOST_IPC_IN_19] in region 0 ... 41: SYSTEM: ListElem Shared Addr = 0x2b17a680 42: SYSTEM: Creating ListMP [HOST_IPC_OUT_20] in region 0 ... 44: SYSTEM: Creating ListMP [HOST_IPC_IN_20] in region 0 ... 46: SYSTEM: ListElem Shared Addr = 0x2b19a080 47: SYSTEM: Creating ListMP [HOST_IPC_OUT_21] in region 0 ... 49: SYSTEM: Creating ListMP [HOST_IPC_IN_21] in region 0 ... 51: SYSTEM: ListElem Shared Addr = 0x2b1b9a80 67: SYSTEM: System Common Init Done !!! [FBDEV] [FBDEV] FB: Starting !!! [FBDEV] FB: Opened device [/dev/fb0] (fd=20) !!! [FBDEV] [FBDEV] Fix Screen Info [FBDEV] --------------- [FBDEV] Line Length - 3840 [FBDEV] Physical Address = fea00000 [FBDEV] Buffer Length = 8294400 [FBDEV] [FBDEV] [FBDEV] Var Screen Info [FBDEV] --------------- [FBDEV] Xres - 1920 [FBDEV] Yres - 1080 [FBDEV] Xres Virtual - 1920 [FBDEV] Yres Virtual - 1080 [FBDEV] Bits Per Pixel - 16 [FBDEV] Pixel Clk - 6734 [FBDEV] Rotation - 0 [FBDEV] [FBDEV] [FBDEV] Reg Params Info [FBDEV] --------------- [FBDEV] region 0, postion 0 x 0, prioirty 1 [FBDEV] first 1, last 1 [FBDEV] sc en 0, sten en 0 [FBDEV] tran en 0, type 0, key 0 [FBDEV] blend 0, alpha 0 [FBDEV] bb en 0, alpha 0 [FBDEV] [FBDEV] [FBDEV] ### BUF SIZE = 4147200 Bytes !!! [FBDEV] [FBDEV] [FBDEV] Fix Screen Info [FBDEV] --------------- [FBDEV] Line Length - 3840 [FBDEV] Physical Address = fea00000 [FBDEV] Buffer Length = 8294400 [FBDEV] [FBDEV] [FBDEV] Var Screen Info [FBDEV] --------------- [FBDEV] Xres - 1920 [FBDEV] Yres - 1080 [FBDEV] Xres Virtual - 1920 [FBDEV] Yres Virtual - 1080 [FBDEV] Bits Per Pixel - 16 [FBDEV] Pixel Clk - 6734 [FBDEV] Rotation - 0 [FBDEV] [FBDEV] [FBDEV] Reg Params Info [FBDEV] --------------- [FBDEV] region 0, postion 0 x 0, prioirty 1 [FBDEV] first 1, last 1 [FBDEV] sc en 0, sten en 0 [FBDEV] tran en 0, type 0, key 0 [FBDEV] blend 0, alpha 0 [FBDEV] bb en 0, alpha 0 [FBDEV] [FBDEV] [FBDEV] ### BUF SIZE = 4147200 Bytes !!! [FBDEV] [FBDEV] grpx_fb_draw ... [FBDEV] grpx_fb_draw ... Done !!! [FBDEV] FB: Start DONE !!! [FBDEV] 177: MCFW : CPU Revision [ES2.0] !!! 177: MCFW : Detected [(null)] Board !!! 177: MCFW : Base Board Revision [DVR] !!! 177: MCFW : Daughter Card Revision [DVR] !!! [m3vpss ] 38671: CAPTURE: Create in progress !!! [m3vpss ] 38700: CAPTURE: VIP0 PortA capture mode is [16-bit, Non-mux Embedded Sync] !!! [m3vpss ] 38793: CAPTURE: VIP1 PortA capture mode is [16-bit, Non-mux Embedded Sync] !!! [m3vpss ] UTILS: DMA: Allocated CH (TCC) = 58 (58) [m3vpss ] CAPTURE::HEAPID:0 USED:608 [m3vpss ] CAPTURE::HEAPID:4 USED:44697600 [m3vpss ] 38887: CAPTURE: Create Done !!! [m3vpss ] 38888: NSF: Create in progress !!! [m3vpss ] NSF::HEAPID:0 USED:128 [m3vpss ] NSF::HEAPID:1 USED:6336 [m3vpss ] NSF::HEAPID:4 USED:19783680 [m3vpss ] 38980: NSF: Create Done !!! [m3vpss ] 38980: DEI : Create in progress !!! [m3vpss ] 39026: DEI : Loading Down-scaling Co-effs [m3vpss ] 39026: DEI : Co-effs Loading ... DONE !!! [m3vpss ] DEI:HEAPID:0 USED:64 [m3vpss ] DEI:HEAPID:1 USED:4832 [m3vpss ] DEI:HEAPID:4 USED:9676800 [m3vpss ] 39027: DEI : Create Done !!! [m3vpss ] 39027: DEI : Create in progress !!! [m3vpss ] 39073: DEI : Loading Down-scaling Co-effs [m3vpss ] 39073: DEI : Co-effs Loading ... DONE !!! [m3vpss ] DEI:HEAPID:0 USED:64 [m3vpss ] DEI:HEAPID:1 USED:4704 [m3vpss ] DEI:HEAPID:4 USED:9676800 [m3vpss ] 39073: DEI : Create Done !!! [m3vpss ] 39074: NULL_SRC: Create in progress !!! [m3vpss ] 39081: NULL_SRC: Create Done !!! [m3vpss ] 39082: MERGE : Create Done !!! [m3vpss ] 39085: DUP : Create Done !!! [m3vpss ] 39085: SWMS: Create in progress !!! [m3vpss ] UTILS: DMA: Allocated CH (TCC) = 59 (59) [m3vpss ] SWMS: instance 0, sc id 5, start win 0 end win 17 [m3vpss ] 39187: SWMS0 : Loading Vertical Co-effs (UPSCALE)x ... [m3vpss ] 39187: SWMS0 : Loading Horizontal Co-effs (UPSCALE)x ... [m3vpss ] 39187: SWMS : Co-effs Loading ... DONE !!! [m3vpss ] AVSYNC:WARNING!! Application wrongly configureddisplayID[-1]. Reseting to correct displayID[0] [m3vpss ] 39188: SWMS : ******* Configuring clock 30 secs... [m3vpss ] 39188: SWMS0 : Loading Vertical Co-effs (UPSCALE)x ... [m3vpss ] 39188: SWMS0 : Loading Horizontal Co-effs (UPSCALE)x ... [m3vpss ] 39188: SWMS : Co-effs Loading ... DONE !!! [m3vpss ] [m3vpss ] *** [SWMS0] Mosaic Parameters *** [m3vpss ] [m3vpss ] Output FPS: 30 [m3vpss ] [m3vpss ] Win | Ch | Input | Input | Input | Input | Output | Output | Output | Output | Low Cost | SWMS | Data | Blank | [m3vpss ] Num | Num | Start X, Y | Width x Height | Pitch Y / C | Memory Type | Start X, Y | Width x Height | Pitch Y / C | Memory Type | ON / OFF | Inst | Format| Frame | [m3vpss ] ---------------------------------------------------------------------------------------------------------------------------------------------------------------------- [m3vpss ] 0 | 0 | 0, 0 | 1280 x 720 | 1280 / 1280 | NON-TILED | 0, 0 | 1920 x 1080 | 3840 / 0 | NON-TILED | OFF | 0 | 420SP | OFF | [m3vpss ] [m3vpss ] SWMS:HEAPID:0 USED:360 [m3vpss ] SWMS:HEAPID:1 USED:47296 [m3vpss ] SWMS:HEAPID:4 USED:20736000 [m3vpss ] 39190: SWMS: Create Done !!! [m3vpss ] 39190: SWMS: Create in progress !!! [m3vpss ] UTILS: DMA: Allocated CH (TCC) = 60 (60) [m3vpss ] SWMS: instance 0, sc id 5, start win 0 end win 17 [m3vpss ] 39292: SWMS1 : Loading Vertical Co-effs (UPSCALE)x ... [m3vpss ] 39292: SWMS1 : Loading Horizontal Co-effs (UPSCALE)x ... [m3vpss ] 39292: SWMS : Co-effs Loading ... DONE !!! [m3vpss ] AVSYNC:WARNING!! Application wrongly configureddisplayID[-1]. Reseting to correct displayID[1] [m3vpss ] 39293: SWMS : ******* Configuring clock 30 secs... [m3vpss ] 39293: SWMS1 : Loading Vertical Co-effs (UPSCALE)x ... [m3vpss ] 39293: SWMS1 : Loading Horizontal Co-effs (UPSCALE)x ... [m3vpss ] 39293: SWMS : Co-effs Loading ... DONE !!! [m3vpss ] [m3vpss ] *** [SWMS1] Mosaic Parameters *** [m3vpss ] [m3vpss ] Output FPS: 30 [m3vpss ] [m3vpss ] Win | Ch | Input | Input | Input | Input | Output | Output | Output | Output | Low Cost | SWMS | Data | Blank | [m3vpss ] Num | Num | Start X, Y | Width x Height | Pitch Y / C | Memory Type | Start X, Y | Width x Height | Pitch Y / C | Memory Type | ON / OFF | Inst | Format| Frame | [m3vpss ] ---------------------------------------------------------------------------------------------------------------------------------------------------------------------- [m3vpss ] 0 | 0 | 0, 0 | 1280 x 720 | 1280 / 1280 | NON-TILED | 0, 0 | 1920 x 1080 | 3840 / 0 | NON-TILED | OFF | 0 | 420SP | OFF | [m3vpss ] [m3vpss ] SWMS:HEAPID:0 USED:360 [m3vpss ] SWMS:HEAPID:1 USED:43776 [m3vpss ] SWMS:HEAPID:4 USED:20736000 [m3vpss ] 39294: SWMS: Create Done !!! [m3vpss ] 39295: DISPLAY: Create in progress !!! [m3vpss ] 39296: DISPLAY: Create Done !!! [m3vpss ] 39296: DISPLAY: Create in progress !!! [m3vpss ] 39297: DISPLAY: Create Done !!! [m3vpss ] 39298: DISPLAY: Start in progress !!! [m3vpss ] 39343: DISPLAY: Start Done !!! [m3vpss ] 39343: DISPLAY: HDDAC(BP0) : 44 fps, Latency (Min / Max) = ( 255 / 0 ), Callback Interval (Min / Max) = ( 255 / 0 ) !!! [m3vpss ] 39343: DISPLAY: UNDERFLOW COUNT: HDMI(BP0) 1, HDDAC(BP0) 1, DVO2(BP1) 0, SDDAC(SEC1) 1 [m3vpss ] 39344: SYSTEM : FREE SPACE : System Heap = 5576 B, Mbx = 10238 msgs) [m3vpss ] 39344: SYSTEM : FREE SPACE : SR0 Heap = 11003648 B (10 MB) [m3vpss ] 39344: SYSTEM : FREE SPACE : Frame Buffer = 114824064 B (109 MB) [m3vpss ] 39344: SYSTEM : FREE SPACE : Bitstream Buffer = 352845696 B (336 MB) [m3vpss ] 39344: DISPLAY: Start in progress !!! [m3vpss ] 39345: SYSTEM : FREE SPACE : Tiler 8-bit = 134217728 B (128 MB) - TILER ON [m3vpss ] 39345: SYSTEM : FREE SPACE : Tiler 16-bit = 134217728 B (128 MB) - TILER ON [m3vpss ] 39398: DISPLAY: Start Done !!! [m3vpss ] 39398: DISPLAY: DVO2(BP1) : 37 fps, Latency (Min / Max) = ( 255 / 0 ), Callback Interval (Min / Max) = ( 255 / 0 ) !!! [m3vpss ] 39398: SWMS: Start in Progress !!! [m3vpss ] 39398: SWMS: Start Done !!! [m3vpss ] 39399: SWMS: Start in Progress !!! [m3vpss ] 39399: SWMS: Start Done !!! [m3vpss ] 39400: NULL_SRC: Start Done !!! [m3vpss ] 39400: CAPTURE: Start in progress !!! [m3vpss ] 39400: CAPTURE: Start Done !!! ============= Run-Time Menu ============= 1: Capture Settings 2: Encode Settings 3: Decode Settings 4: Display Settings 5: Audio Capture / Playback Settings 6: Audio Capture <TVP5158> & Encode <AAC-LC> demo 7: Audio encode demo <AAC-LC File In/Out> 8: Audio decode demo <AAC-LC File In/Out> i: Print detailed system information s: Core Status: Active/In-active f: Switch IVA Channel Map e: Stop Demo Enter Choice: i [m3vpss ] [m3vpss ] *** Capture Driver Advanced Statistics *** [m3vpss ] [m3vpss ] *** [NSF0] NSF Statistics *** [m3vpss ] [m3vpss ] Elasped Time : 28 secs [m3vpss ] Total Fields Processed : 3377 [m3vpss ] Total Fields FPS : 222 FPS [m3vpss ] [m3vpss ] [m3vpss ] CH | In Recv In Reject In Process Out User Out Out [m3vpss ] Num | FPS FPS FPS FPS Skip FPS Skip FPS [m3vpss ] ------------------------------------------------ [m3vpss ] 0 | 60 0 60 60 0 0 [m3vpss ] 1 | 60 0 60 60 0 0 [m3vpss ] [m3vpss ] [m3vpss ] VIP Parser Reset Count : 0 [m3vpss ] [m3vpss ] | Total Even Odd Total Even Odd Min / Max Min / Max Dropped Fid Repeat Frame Error Y/C [m3vpss ] CH | Fields Fields Fields FPS FPS FPS Width Height Fields Count (Desc Error Y/C) [m3vpss ] ------------------------------------------------------------------------------------------------------------ [m3vpss ] 000 | 1690 1690 0 60 60 0 1280 / 1280 720 / 720 1 0 0/0 (0/0) [m3vpss ] 200 | 1690 1690 0 60 60 0 1280 / 1280 720 / 720 1 0 0/0 (0/0) [m3vpss ] [m3vpss ] VIP Capture Port 0 | DescMissMatch1 = 0, DescMissMatch2 = 0 , DescMissMatch3 = 0 [m3vpss ] VIP Capture Port 2 | DescMissMatch1 = 0, DescMissMatch2 = 0 , DescMissMatch3 = 0 [m3vpss ] [m3vpss ] *** Capture List Manager Advanced Statistics *** [m3vpss ] [m3vpss ] List Post Count : 7045 [m3vpss ] List Stall Count : 0 [m3vpss ] List Post Time (ms) : Max = 0, Min = 0, Avg = 0, Total = 0 [m3vpss ] INTC Timeout Count : (0, 0) (Min timeout value = 979, 993) [m3vpss ] Descriptor miss found count : 0 [m3vpss ] [m3vpss ] [m3vpss ] VIP and VPDMA registers, [m3vpss ] VIP0 : FIQ_STATUS : 0x4810551c = 0x00004400 [m3vpss ] VIP1 : FIQ_STATUS : 0x48105a1c = 0x00004400 [m3vpss ] VPDMA: LIST_BUSY : 0x4810d00c = 0x00060000 [m3vpss ] [m3vpss ] [m3vpss ] 67687: CAPTURE: Fields = 3377 (fps = 119, CPU Load = 0) [m3vpss ] 67687: CAPTURE: Num Resets = 0 (Avg 0 ms per reset) [m3vpss ] 67687: SYSTEM : FREE SPACE : System Heap = 5576 B, Mbx = 10239 msgs) [m3vpss ] 67687: SYSTEM : FREE SPACE : SR0 Heap = 11003648 B (10 MB) [m3vpss ] 67688: SYSTEM : FREE SPACE : Frame Buffer = 114824064 B (109 MB) [m3vpss ] 67688: SYSTEM : FREE SPACE : Bitstream Buffer = 352845696 B (336 MB) [m3vpss ] 67689: SYSTEM : FREE SPACE : Tiler 8-bit = 134217728 B (128 MB) - TILER ON [m3vpss ] 67689: SYSTEM : FREE SPACE : Tiler 16-bit = 134217728 B (128 MB) - TILER ON [m3vpss ] [m3vpss ] *** [DEI0 ] DEI Statistics *** [m3vpss ] [m3vpss ] Elasped Time : 30 secs [m3vpss ] Total Fields Processed : 1 [m3vpss ] Total Fields FPS : 0 FPS [m3vpss ] [m3vpss ] [m3vpss ] CH | In Recv In Reject In Process Out[0] Out[1] Out[2] Out[3] Out[4] Skip Out[0] Skip Out[1] Skip Out[2] Skip Out[3] Skip Out[4] User Out[0] User Out[1] User Out[2] User Out[3] User Out[4] Latency [m3vpss ] Num | FPS FPS FPS FPS FPS FPS FPS FPS FPS FPS FPS FPS FPS Skip FPS Skip FPS Skip FPS Skip FPS Skip FPS Min / Max [m3vpss ] ------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------- [m3vpss ] 0 | 60 60 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 10 / 10 [m3vpss ] [m3vpss ] [m3vpss ] *** [DEI2 ] DEI Statistics *** [m3vpss ] [m3vpss ] Elasped Time : 30 secs [m3vpss ] Total Fields Processed : 1 [m3vpss ] Total Fields FPS : 0 FPS [m3vpss ] [m3vpss ] [m3vpss ] CH | In Recv In Reject In Process Out[0] Out[1] Out[2] Out[3] Out[4] Skip Out[0] Skip Out[1] Skip Out[2] Skip Out[3] Skip Out[4] User Out[0] User Out[1] User Out[2] User Out[3] User Out[4] Latency [m3vpss ] Num | FPS FPS FPS FPS FPS FPS FPS FPS FPS FPS FPS FPS FPS Skip FPS Skip FPS Skip FPS Skip FPS Skip FPS Min / Max [m3vpss ] ------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------- [m3vpss ] 0 | 60 60 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 14 / 14 [m3vpss ] [m3vpss ] [m3vpss ] *** [SWMS0] Mosaic Statistics *** [m3vpss ] [m3vpss ] Elasped Time: 30 secs [m3vpss ] [m3vpss ] Output Request FPS : 33 fps (1006 frames) [m3vpss ] Output Actual FPS : 33 fps (1006 frames) [m3vpss ] Output Drop FPS : 0 fps (0 frames) [m3vpss ] Output Reject FPS : 0 fps (0 frames) [m3vpss ] Scaling Internal : 30 ms [m3vpss ] Scaling Internal min : 5 ms [m3vpss ] Scaling Internal max : 51 ms [m3vpss ] [m3vpss ] Win | Window Repeat Drop Recv Que FID Invlid Acc Event Invalid Que Reject Reject Latency [m3vpss ] Num | FPS FPS FPS FPS FPS FPS Count (Max/Min) CH Frames Frames Frames Min / Max [m3vpss ] ------------------------------------------------------------------------------------------------------ [m3vpss ] 0 | 33 33 0 0 0 0 0 ( 0/255) 0 0 0 62 / 30126 [m3vpss ] [m3vpss ] [m3vpss ] *** [SWMS0] Mosaic Parameters *** [m3vpss ] [m3vpss ] Output FPS: 30 [m3vpss ] [m3vpss ] Win | Ch | Input | Input | Input | Input | Output | Output | Output | Output | Low Cost | SWMS | Data | Blank | [m3vpss ] Num | Num | Start X, Y | Width x Height | Pitch Y / C | Memory Type | Start X, Y | Width x Height | Pitch Y / C | Memory Type | ON / OFF | Inst | Format| Frame | [m3vpss ] ---------------------------------------------------------------------------------------------------------------------------------------------------------------------- [m3vpss ] 0 | 0 | 0, 0 | 1280 x 720 | 1280 / 1280 | NON-TILED | 0, 0 | 1920 x 1080 | 3840 / 0 | NON-TILED | OFF | 0 | 420SP | OFF | [m3vpss ] [m3vpss ] [m3vpss ] [m3vpss ] *** [SWMS1] Mosaic Statistics *** [m3vpss ] [m3vpss ] Elasped Time: 30 secs [m3vpss ] [m3vpss ] Output Request FPS : 33 fps (1005 frames) [m3vpss ] Output Actual FPS : 33 fps (1005 frames) [m3vpss ] Output Drop FPS : 0 fps (0 frames) [m3vpss ] Output Reject FPS : 0 fps (0 frames) [m3vpss ] Scaling Internal : 30 ms [m3vpss ] Scaling Internal min : 23 ms [m3vpss ] Scaling Internal max : 47 ms [m3vpss ] [m3vpss ] Win | Window Repeat Drop Recv Que FID Invlid Acc Event Invalid Que Reject Reject Latency [m3vpss ] Num | FPS FPS FPS FPS FPS FPS Count (Max/Min) CH Frames Frames Frames Min / Max [m3vpss ] ------------------------------------------------------------------------------------------------------ [m3vpss ] 0 | 33 33 0 0 0 0 0 ( 0/255) 0 0 0 71 / 30127 [m3vpss ] [m3vpss ] [m3vpss ] *** [SWMS1] Mosaic Parameters *** [m3vpss ] [m3vpss ] Output FPS: 30 [m3vpss ] [m3vpss ] Win | Ch | Input | Input | Input | Input | Output | Output | Output | Output | Low Cost | SWMS | Data | Blank | [m3vpss ] Num | Num | Start X, Y | Width x Height | Pitch Y / C | Memory Type | Start X, Y | Width x Height | Pitch Y / C | Memory Type | ON / OFF | Inst | Format| Frame | [m3vpss ] ---------------------------------------------------------------------------------------------------------------------------------------------------------------------- [m3vpss ] 0 | 0 | 0, 0 | 1280 x 720 | 1280 / 1280 | NON-TILED | 0, 0 | 1920 x 1080 | 3840 / 0 | NON-TILED | OFF | 0 | 420SP | OFF | [m3vpss ] [m3vpss ] [m3vpss ] 69696: DISPLAY: HDDAC(BP0) : 59 fps, Latency (Min / Max) = ( 2 / 66 ), Callback Interval (Min / Max) = ( 16 / 17 ) !!! [m3vpss ] 69696: DISPLAY: UNDERFLOW COUNT: HDMI(BP0) 1821, HDDAC(BP0) 1823, DVO2(BP1) 1823, SDDAC(SEC1) 3697 [m3vpss ] 69696: SYSTEM : FREE SPACE : System Heap = 5576 B, Mbx = 10239 msgs) [m3vpss ] 69696: SYSTEM : FREE SPACE : SR0 Heap = 11003648 B (10 MB) [m3vpss ] 69696: SYSTEM : FREE SPACE : Frame Buffer = 114824064 B (109 MB) [m3vpss ] 69697: SYSTEM : FREE SPACE : Bitstream Buffer = 352845696 B (336 MB) [m3vpss ] 69697: SYSTEM : FREE SPACE : Tiler 8-bit = 134217728 B (128 MB) - TILER ON [m3vpss ] 69697: SYSTEM : FREE SPACE : Tiler 16-bit = 134217728 B (128 MB) - TILER ON [m3vpss ] 69699: DISPLAY: DVO2(BP1) : 59 fps, Latency (Min / Max) = ( 6 / 60 ), Callback Interval (Min / Max) = ( 16 / 17 ) !!! [m3vpss ] [m3vpss ] 75701: LOAD: CPU: 15.2% HWI: 2.4%, SWI:1.4% [m3vpss ] [m3vpss ] 75701: LOAD: TSK: CAPTURE : 0.6% [m3vpss ] 75701: LOAD: TSK: NSF0 : 1.0% [m3vpss ] 75702: LOAD: TSK: DEI0 : 0.2% [m3vpss ] 75702: LOAD: TSK: DEI2 : 0.3% [m3vpss ] 75702: LOAD: TSK: DISPLAY0 : 0.4% [m3vpss ] 75703: LOAD: TSK: DISPLAY1 : 0.3% [m3vpss ] 75703: LOAD: TSK: NULL_SRC0 : 0.2% [m3vpss ] 75703: LOAD: TSK: DUP0 : 0.7% [m3vpss ] 75703: LOAD: TSK: SWMS0 : 1.8% [m3vpss ] 75703: LOAD: TSK: SWMS1 : 2.7% [m3vpss ] 75703: LOAD: TSK: MERGE0 : 0.2% [m3vpss ] 75703: LOAD: TSK: MISC : 3.0% [m3vpss ] [m3video] [m3video] 76204: LOAD: CPU: 0.8% HWI: 0.4%, SWI:0.2% [m3video] [m3video] 76204: LOAD: TSK: MISC : 0.2% [m3video] [c6xdsp ] [c6xdsp ] 75076: LOAD: CPU: 0.1% HWI: 0.0%, SWI:0.0% [c6xdsp ] [c6xdsp ] 75076: LOAD: TSK: MISC : 0.1% [c6xdsp ] ============= Run-Time Menu ============= 1: Capture Settings 2: Encode Settings 3: Decode Settings 4: Display Settings 5: Audio Capture / Playback Settings 6: Audio Capture <TVP5158> & Encode <AAC-LC> demo 7: Audio encode demo <AAC-LC File In/Out> 8: Audio decode demo <AAC-LC File In/Out> i: Print detailed system information s: Core Status: Active/In-active f: Switch IVA Channel Map e: Stop Demo Enter Choice:
and more information ,like create time parameters ,you can see in test.txt
now ,when i run this demo, we can only see one picture on screen and never changed . i dont know why ,
can you help me ?thank you!
sometimes if we pull out hdmi input and then plug in , the pitcture on screen may be changed ,but also only one piture can show.
but when we stop this demo ,and exit demo, then we restart demo and restart vcap_vdis , we can see another piture, which is now captured.but still never changed.