This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Kernel panic on Sitara EVM based custom board

Other Parts Discussed in Thread: AM3354

We have made a custom board based on the AM335X sitara EVM design. We have tried our maximum to use the same components used in the reference design except the MPU for which we use Sitara AM3354.  It is running TI provided rowboat android 4.0.3. Occasionally we are seeing a crash. I am clueless about whats causing it. I have attached the bootlog.  Please check it out and let me know if you find anything regarding the crash.

CCCCCCCC                                                                                    
U-Boot SPL 2011.09 (Jun 10 2013 - 15:24:26)                                                 
Texas Instruments Revision detection unimplemented                                          
header.magic = ee3355aa                                                                     
header.magic = ee3355aa                                                                     
No daughter card present                                                                    
OMAP SD/MMC: 0                                                                              
reading u-boot.img                                                                          
reading u-boot.img                                                                          
                                                                                            
                                                                                            
U-Boot 2011.09 (Jun 10 2013 - 15:24:26)                                                     
                                                                                            
I2C:   ready                                                                                
DRAM:  256 MiB                                                                              
WARNING: Caches not enabled                                                                 
header.magic = ee3355aa                                                                     
No daughter card present                                                                    
NAND:  HW ECC Hamming Code selected                                                         
No NAND device found!!!                                                                     
0 MiB                                                                                       
MMC:   OMAP SD/MMC: 0, OMAP SD/MMC: 1                                                       
*** Warning - readenv() failed, using default environment                                   
                                                                                            
Net:   cpsw                                                                                 
Hit any key to stop autoboot:  0                                                            
SD/MMC found on device 0                                                                    
reading uEnv.txt                                                                            
                                                                                            
223 bytes read                                                                              
Loaded environment from uEnv.txt                                                            
Importing environment from mmc ...                                                          
Running uenvcmd ...                                                                         
reading uImage                                                                              
                                                                                            
3689128 bytes read                                                                          
## Booting kernel from Legacy Image at 81000000 ...                                         
   Image Name:   Linux-3.2.0                                                                
   Image Type:   ARM Linux Kernel Image (uncompressed)                                      
   Data Size:    3689064 Bytes = 3.5 MiB                                                    
   Load Address: 80008000                                                                   
   Entry Point:  80008000                                                                   
   Verifying Checksum ... OK                                                                
   Loading Kernel Image ... OK                                                              
OK                                                                                          
                                                                                            
Starting kernel ...                                                                         
                                                                                            
Uncompressing Linux... done, booting the kernel.                                            
[    0.000000] Linux version 3.2.0 (cdl@cdl) (gcc version 4.5.3 20110311 (prerelease) (GCC)3
[    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d              
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache     
[    0.000000] Machine: am335xevm                                                           
[    0.000000] Memory policy: ECC disabled, Data cache writeback                            
[    0.000000] On node 0 totalpages: 65536                                                  
[    0.000000] free_area_init_node: node 0, pgdat c073b094, node_mem_map c086d000           
[    0.000000]   Normal zone: 512 pages used for memmap                                     
[    0.000000]   Normal zone: 0 pages reserved                                              
[    0.000000]   Normal zone: 65024 pages, LIFO batch:15                                    
[    0.000000] AM335X ES1.0 (sgx neon )                                                     
[    0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768                                
[    0.000000] pcpu-alloc: [0] 0                                                            
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 65024   
[    0.000000] Kernel command line: console=ttyO0,115200n8 androidboot.console=ttyO0 mem=25f
[    0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)                          
[    0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)              
[    0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)                
[    0.000000] Memory: 256MB = 256MB total                                                  
[    0.000000] Memory: 251228k/251228k available, 10916k reserved, 0K highmem               
[    0.000000] Virtual kernel memory layout:                                                
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)                            
[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)                            
[    0.000000]     vmalloc : 0xd0800000 - 0xff000000   ( 744 MB)                            
[    0.000000]     lowmem  : 0xc0000000 - 0xd0000000   ( 256 MB)                            
[    0.000000]     modules : 0xbf000000 - 0xc0000000   (  16 MB)                            
[    0.000000]       .text : 0xc0008000 - 0xc06a1000   (6756 kB)                            
[    0.000000]       .init : 0xc06a1000 - 0xc06e0000   ( 252 kB)                            
[    0.000000]       .data : 0xc06e0000 - 0xc073b840   ( 367 kB)                            
[    0.000000]        .bss : 0xc073b864 - 0xc086cc98   (1222 kB)                            
[    0.000000] NR_IRQS:396                                                                  
[    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts          
[    0.000000] Total of 128 interrupts on 1 active controller                               
[    0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz                              
[    0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz                                       
[    0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms   
[    0.000000] Console: colour dummy device 80x30                                           
[    0.000152] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)                      
[    0.058959] pid_max: default: 32768 minimum: 301                                         
[    0.059082] Security Framework initialized                                               
[    0.059143] Mount-cache hash table entries: 512                                          
[    0.059509] CPU: Testing write buffer coherency: ok                                      
[    0.061431] ttyO0 used as console in debug mode uart0 clocks will not be gated           
[    0.079406] omap_hwmod: pruss: failed to hardreset                                       
[    0.080169] print_constraints: dummy:                                                    
[    0.080383] NET: Registered protocol family 16                                           
[    0.081451] OMAP GPIO hardware version 0.1                                               
[    0.082489] omap_mux_init: Add partition: #1: core, flags: 0                             
[    0.083618] omap_mux_init_signal: Setting signal xdma_event_intr1.clkout2 0x0027 -> 0x003
[    0.083709]  omap_i2c.1: alias fck already exists                                        
[    0.084228]  omap2_mcspi.1: alias fck already exists                                     
[    0.084350]  omap2_mcspi.2: alias fck already exists                                     
[    0.084503]  edma.0: alias fck already exists                                            
[    0.084503]  edma.0: alias fck already exists                                            
[    0.084533]  edma.0: alias fck already exists                                            
[    0.094146] bio: create slab <bio-0> at 0                                                
[    0.095123] SCSI subsystem initialized                                                   
[    0.095916] usbcore: registered new interface driver usbfs                               
[    0.096038] usbcore: registered new interface driver hub                                 
[    0.096191] usbcore: registered new device driver usb                                    
[    0.096313] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3               
[    0.096466] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1               
[    0.096893] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz                               
[    0.098144] tps65910 1-002d: JTAGREVNUM 0x0                                              
[    0.100341] print_constraints: VRTC:                                                     
[    0.101684] print_constraints: VIO: at 1500 mV                                           
[    0.103881] print_constraints: VDD1: 600 <--> 1500 mV at 1262 mV normal                  
[    0.106048] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal                  
[    0.106964] print_constraints: VDD3: 5000 mV                                             
[    0.108276] print_constraints: VDIG1: at 1800 mV                                         
[    0.109619] print_constraints: VDIG2: at 1800 mV                                         
[    0.110961] print_constraints: VPLL: at 1800 mV                                          
[    0.112274] print_constraints: VDAC: at 1800 mV                                          
[    0.113586] print_constraints: VAUX1: at 1800 mV                                         
[    0.114929] print_constraints: VAUX2: at 3300 mV                                         
[    0.116241] print_constraints: VAUX33: at 3300 mV                                        
[    0.117584] print_constraints: VMMC: at 3300 mV                                          
[    0.117858] tps65910 1-002d: No interrupt support, no core IRQ                           
[    0.118377] Advanced Linux Sound Architecture Driver Version 1.0.24.                     
[    0.118957] Bluetooth: Core ver 2.16                                                     
[    0.119049] NET: Registered protocol family 31                                           
[    0.119049] Bluetooth: HCI device and connection manager initialized                     
[    0.119079] Bluetooth: HCI socket layer initialized                                      
[    0.119079] Bluetooth: L2CAP socket layer initialized                                    
[    0.119140] Bluetooth: SCO socket layer initialized                                      
[    0.119323] Switching to clocksource gp timer                                            
[    0.127044] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)                         
[    0.127227] musb-hdrc musb-hdrc.0: dma type: pio                                         
[    0.127380] MUSB0 controller's USBSS revision = 4ea20800                                 
[    0.127441] musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-)
[    0.127441] musb-hdrc: MHDRC RTL version 2.0                                             
[    0.127471] musb-hdrc: setup fifo_mode 4                                                 
[    0.127502] musb-hdrc: 28/31 max ep, 16384/16384 memory                                  
[    0.127838] musb-hdrc musb-hdrc.0: USB OTG mode controller at d083c000 using PIO, IRQ 18 
[    0.128082] musb-hdrc musb-hdrc.1: dma type: pio                                         
[    0.128234] MUSB1 controller's USBSS revision = 4ea20800                                 
[    0.128265] musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-)
[    0.128265] musb-hdrc: MHDRC RTL version 2.0                                             
[    0.128295] musb-hdrc: setup fifo_mode 4                                                 
[    0.128326] musb-hdrc: 28/31 max ep, 16384/16384 memory                                  
[    0.128356] musb-hdrc musb-hdrc.1: MUSB HDRC host driver                                 
[    0.128417] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1         
[    0.128540] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002                
[    0.128570] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1           
[    0.128570] usb usb1: Product: MUSB HDRC host driver                                     
[    0.128601] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd                                 
[    0.128601] usb usb1: SerialNumber: musb-hdrc.1                                          
[    0.129180] hub 1-0:1.0: USB hub found                                                   
[    0.129211] hub 1-0:1.0: 1 port detected                                                 
[    0.129669] musb-hdrc musb-hdrc.1: USB Host mode controller at d083e800 using PIO, IRQ 19
[    0.130004] NET: Registered protocol family 2                                            
[    0.130187] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)               
[    0.130584] TCP established hash table entries: 8192 (order: 4, 65536 bytes)             
[    0.130737] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)                    
[    0.130828] TCP: Hash tables configured (established 8192 bind 8192)                     
[    0.130859] TCP reno registered                                                          
[    0.130859] UDP hash table entries: 256 (order: 0, 4096 bytes)                           
[    0.130889] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)                      
[    0.131072] NET: Registered protocol family 1                                            
[    0.131317] RPC: Registered named UNIX socket transport module.                          
[    0.131347] RPC: Registered udp transport module.                                        
[    0.131347] RPC: Registered tcp transport module.                                        
[    0.131347] RPC: Registered tcp NFSv4.1 backchannel transport module.                    
[    0.131591] NetWinder Floating Point Emulator V0.97 (double precision)                   
[    0.259185] ashmem: initialized                                                          
[    0.259429] VFS: Disk quotas dquot_6.5.2                                                 
[    0.259552] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)                   
[    0.260437] msgmni has been set to 490                                                   
[    0.261413] io scheduler noop registered                                                 
[    0.261413] io scheduler deadline registered                                             
[    0.261505] io scheduler cfq registered (default)                                        
[    0.262084] Could not set LED4 to fully on                                               
[    0.263275] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0             
[    1.016632] console [ttyO0] enabled                                                      
[    1.020660] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1             
[    1.028320] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2             
[    1.035949] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3             
[    1.043762] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4             
[    1.051422] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5             
[    1.065093] brd: module loaded                                                           
[    1.071472] loop: module loaded                                                          
[    1.074951] i2c-core: driver [tsl2550] using legacy suspend method                       
[    1.081420] i2c-core: driver [tsl2550] using legacy resume method                        
[    1.087829] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write              
[    1.150024] No daughter card found on AM335x EVM                                         
[    1.154876] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write              
[    1.164215] Board name: A335X_SK                                                         
[    1.167572] Board version: 1.2B                                                          
[    1.170867] Akhil-setup_startupkit()                                                     
[    1.174407] The board is a AM335x Starter Kit.                                           
[    1.179290] omap_mux_init_signal: Setting signal mii1_rxd2.mmc1_dat3 0x0022 -> 0x0034    
[    1.187469] omap_mux_init_signal: Setting signal mii1_rxd3.mmc1_dat2 0x0022 -> 0x0034    
[    1.195648] omap_mux_init_signal: Setting signal mii1_rxclk.mmc1_dat1 0x0022 -> 0x0034   
[    1.203918] omap_mux_init_signal: Setting signal mii1_txclk.mmc1_dat0 0x0002 -> 0x0034   
[    1.212188] omap_mux_init_signal: Setting signal mii1_txd0.mmc1_clk 0x0002 -> 0x0036     
[    1.220275] omap_mux_init_signal: Setting signal mii1_txd1.mmc1_cmd 0x0002 -> 0x0036     
[    1.228363] omap_mux_init_signal: Setting signal mmc0_dat3.mmc0_dat3 0x0030 -> 0x0030    
[    1.236541] omap_mux_init_signal: Setting signal mmc0_dat2.mmc0_dat2 0x0030 -> 0x0030    
[    1.244720] omap_mux_init_signal: Setting signal mmc0_dat1.mmc0_dat1 0x0030 -> 0x0030    
[    1.252899] omap_mux_init_signal: Setting signal mmc0_dat0.mmc0_dat0 0x0030 -> 0x0030    
[    1.261077] omap_mux_init_signal: Setting signal mmc0_clk.mmc0_clk 0x0030 -> 0x0030      
[    1.269042] omap_mux_init_signal: Setting signal mmc0_cmd.mmc0_cmd 0x0030 -> 0x0030      
[    1.277038] omap_mux_init_signal: Setting signal spi0_cs1.gpio0_6 0x0035 -> 0x0037       
[    1.285034]  omap_hsmmc.0: alias fck already exists                                      
[    1.290344]  omap_hsmmc.1: alias fck already exists                                      
[    1.295593] omap_mux_init_signal: Setting signal usb0_drvvbus.usb0_drvvbus 0x0020 -> 0x00
[    1.304321] omap_mux_init_signal: Setting signal usb1_drvvbus.usb1_drvvbus 0x0020 -> 0x00
[    1.313049] omap_mux_init_signal: Setting signal lcd_data0.lcd_data0 0x002f -> 0x0008    
[    1.321228] omap_mux_init_signal: Setting signal lcd_data1.lcd_data1 0x002f -> 0x0008    
[    1.329406] omap_mux_init_signal: Setting signal lcd_data2.lcd_data2 0x002f -> 0x0008    
[    1.337585] omap_mux_init_signal: Setting signal lcd_data3.lcd_data3 0x002f -> 0x0008    
[    1.345764] omap_mux_init_signal: Setting signal lcd_data4.lcd_data4 0x002f -> 0x0008    
[    1.353942] omap_mux_init_signal: Setting signal lcd_data5.lcd_data5 0x002f -> 0x0008    
[    1.362121] omap_mux_init_signal: Setting signal lcd_data6.lcd_data6 0x002f -> 0x0008    
[    1.370300] omap_mux_init_signal: Setting signal lcd_data7.lcd_data7 0x002f -> 0x0008    
[    1.378479] omap_mux_init_signal: Setting signal lcd_data8.lcd_data8 0x002f -> 0x0008    
[    1.386657] omap_mux_init_signal: Setting signal lcd_data9.lcd_data9 0x002f -> 0x0008    
[    1.394805] omap_mux_init_signal: Setting signal lcd_data10.lcd_data10 0x002f -> 0x0008  
[    1.403167] omap_mux_init_signal: Setting signal lcd_data11.lcd_data11 0x002f -> 0x0008  
[    1.411529] omap_mux_init_signal: Setting signal lcd_data12.lcd_data12 0x002f -> 0x0008  
[    1.419891] omap_mux_init_signal: Setting signal lcd_data13.lcd_data13 0x002f -> 0x0008  
[    1.428253] omap_mux_init_signal: Setting signal lcd_data14.lcd_data14 0x002f -> 0x0008  
[    1.436614] omap_mux_init_signal: Setting signal lcd_data15.lcd_data15 0x002f -> 0x0008  
[    1.444946] omap_mux_init_signal: Setting signal gpmc_ad8.lcd_data16 0x0030 -> 0x0001    
[    1.453125] omap_mux_init_signal: Setting signal gpmc_ad9.lcd_data17 0x0030 -> 0x0001    
[    1.461303] omap_mux_init_signal: Setting signal gpmc_ad10.lcd_data18 0x0030 -> 0x0001   
[    1.469573] omap_mux_init_signal: Setting signal gpmc_ad11.lcd_data19 0x0030 -> 0x0001   
[    1.477844] omap_mux_init_signal: Setting signal gpmc_ad12.lcd_data20 0x0030 -> 0x0001   
[    1.486114] omap_mux_init_signal: Setting signal gpmc_ad13.lcd_data21 0x0030 -> 0x0001   
[    1.494384] omap_mux_init_signal: Setting signal gpmc_ad14.lcd_data22 0x0030 -> 0x0001   
[    1.502655] omap_mux_init_signal: Setting signal gpmc_ad15.lcd_data23 0x0030 -> 0x0001   
[    1.510925] omap_mux_init_signal: Setting signal lcd_vsync.lcd_vsync 0x0027 -> 0x0000    
[    1.519104] omap_mux_init_signal: Setting signal lcd_hsync.lcd_hsync 0x0027 -> 0x0000    
[    1.527252] omap_mux_init_signal: Setting signal lcd_pclk.lcd_pclk 0x0027 -> 0x0000      
[    1.535247] omap_mux_init_signal: Setting signal lcd_ac_bias_en.lcd_ac_bias_en 0x0027 ->0
[    1.544342] omap_mux_init_signal: Setting signal gpmc_a6.gpio1_22 0x0002 -> 0x0007       
[    1.552246] Akhil-LCD_DISEN initialized                                                  
[    1.556488]  da8xx_lcdc.0: alias fck already exists                                      
[    1.561767] da8xx_lcdc da8xx_lcdc.0: GLCD: Found NHD-4.3-ATXI#-T-1 panel                 
[    1.580352] omap_mux_init_signal: Setting signal mcasp0_ahclkr.ecap2_in_pwm2_out 0x0027 4
[    1.589599] omap_mux_init_signal: Setting signal ain0.ain0 0x0028 -> 0x0020              
[    1.596893] omap_mux_init_signal: Setting signal ain1.ain1 0x0028 -> 0x0020              
[    1.604156] omap_mux_init_signal: Setting signal ain2.ain2 0x0028 -> 0x0020              
[    1.611419] omap_mux_init_signal: Setting signal ain3.ain3 0x0028 -> 0x0020              
[    1.618682] omap_mux_init_signal: Setting signal vrefp.vrefp 0x0028 -> 0x0020            
[    1.626129] omap_mux_init_signal: Setting signal vrefn.vrefn 0x0028 -> 0x0020            
[    1.633850] omap_mux_init_signal: Setting signal uart1_ctsn.uart1_ctsn 0x0037 -> 0x0000  
[    1.642242] omap_mux_init_signal: Setting signal uart1_rtsn.uart1_rtsn 0x0037 -> 0x0028  
[    1.650604] omap_mux_init_signal: Setting signal uart1_rxd.uart1_rxd 0x0037 -> 0x0030    
[    1.658752] omap_mux_init_signal: Setting signal uart1_txd.uart1_txd 0x0037 -> 0x0000    
[    1.666931] inside setup_pin_mux of uart4                                                
[    1.671142] omap_mux_init_signal: Setting signal mii1_txd3.uart4_rxd 0x0002 -> 0x0033    
[    1.679290] omap_mux_init_signal: Setting signal mii1_txd2.uart4_txd 0x0002 -> 0x0003    
[    1.687469] uart4 setup done                                                             
[    1.690460] inside setup_pin_mux of uart5                                                
[    1.694671] omap_mux_init_signal: Setting signal mii1_col.uart5_rxd 0x0027 -> 0x0033     
[    1.702758] omap_mux_init_signal: Setting signal mii1_rxdv.uart5_txd 0x0022 -> 0x0003    
[    1.710937] omap_mux_init_signal: Setting signal mii1_crs.uart5_ctsn 0x0027 -> 0x0005    
[    1.719116] omap_mux_init_signal: Setting signal mii1_rxerr.uart5_rtsn 0x0027 -> 0x002d  
[    1.727447] uart5 setup done                                                             
[    1.730468] omap_mux_init_signal: Setting signal gpmc_a7.gpio1_23 0x0022 -> 0x002f       
[    1.738372] omap_mux_init_signal: Setting signal gpmc_csn0.gpio1_29 0x0008 -> 0x0017     
[    1.746459] omap_mux_init_signal: Setting signal mcasp0_ahclkx.gpio3_21 0x0027 -> 0x0007 
[    1.754882] am335xevm: bt init                                                           
[    1.758331] omap_mux_init_signal: Setting signal ecap0_in_pwm0_out.gpio0_7 0x0007 -> 0x07
[    1.767578] (stk) :sysfs entries created                                                 
[    1.771789] (stk) : debugfs entries created                                              
[    1.776947] mtdoops: mtd device (mtddev=name/number) must be supplied                    
[    1.784027] omap2-nand driver initializing                                               
[    1.788360] OneNAND driver initializing                                                  
[    1.792846] CAN device driver interface                                                  
[    1.796844] CAN bus driver for Bosch D_CAN controller 1.0                                
[    1.850006] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6                       
[    1.856475] davinci_mdio davinci_mdio.0: no live phy, scanning all                       
[    1.863159] davinci_mdio: probe of davinci_mdio.0 failed with error -5                   
[    1.870025] PPP generic driver version 2.4.2                                             
[    1.874664] PPP BSD Compression module registered                                        
[    1.879547] PPP Deflate Compression module registered                                    
[    1.884948] usbcore: registered new interface driver cdc_ether                           
[    1.891113] usbcore: registered new interface driver cdc_eem                             
[    1.897064] usbcore: registered new interface driver dm9601                              
[    1.902923] usbcore: registered new interface driver cdc_subset                          
[    1.909149] cdc_ncm: 04-Aug-2011                                                         
[    1.912567] usbcore: registered new interface driver cdc_ncm                             
[    1.918548] usbcore: registered new interface driver cdc_acm                             
[    1.924468] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters  
[    1.932800] Initializing USB Mass Storage driver...                                      
[    1.938018] usbcore: registered new interface driver usb-storage                         
[    1.944305] USB Mass Storage support registered.                                         
[    1.949249] usbcore: registered new interface driver usbserial                           
[    1.955413] USB Serial support registered for generic                                    
[    1.960754] usbcore: registered new interface driver usbserial_generic                   
[    1.967559] usbserial: USB Serial Driver core                                            
[    1.972137] USB Serial support registered for GSM modem (1-port)                         
[    1.978546] usbcore: registered new interface driver option                              
[    1.984375] option: v0.7.2:USB Driver for GSM modems                                     
[    1.991516]  gadget: Mass Storage Function, version: 2009/09/11                          
[    1.997680]  gadget: Number of LUNs=1                                                    
[    2.001525]  lun0: LUN: removable file: (no medium)                                      
[    2.006866]  gadget: android_usb ready                                                   
[    2.010803] musb-hdrc musb-hdrc.0: MUSB HDRC host driver                                 
[    2.016387] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2         
[    2.024230] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002                
[    2.031341] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1           
[    2.038879] usb usb2: Product: MUSB HDRC host driver                                     
[    2.044036] usb usb2: Manufacturer: Linux 3.2.0 musb-hcd                                 
[    2.049591] usb usb2: SerialNumber: musb-hdrc.0                                          
[    2.054809] hub 2-0:1.0: USB hub found                                                   
[    2.058715] hub 2-0:1.0: 1 port detected                                                 
[    2.063476] mousedev: PS/2 mouse device common for all mice                              
[    2.069519] android_work: sent uevent USB_STATE=CONNECTED                                
[    2.075836] input: ti-tsc-adcc as /devices/platform/omap/tsc/input/input0                
[    2.084320] using rtc device, omap_rtc, for alarms                                       
[    2.089172] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0                     
[    2.096099] i2c /dev entries driver                                                      
[    2.099914] Linux video capture interface: v2.00                                         
[    2.104888] usbcore: registered new interface driver uvcvideo                            
[    2.110900] USB Video Class driver (1.1.1)                                               
[    2.116943] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec                         
[    2.123504] device-mapper: uevent: version 1.0.3                                         
[    2.128509] device-mapper: ioctl: 4.22.0-ioctl (2011-10-19) initialised: dm-devel@redhatm
[    2.137329] Bluetooth: HCI UART driver ver 2.2                                           
[    2.141967] Bluetooth: HCI H4 protocol initialized                                       
[    2.146972] Bluetooth: HCILL protocol initialized                                        
[    2.151885] Bluetooth: Bluetooth Driver for TI WiLink - Version 1.0                      
[    2.158477] hdev cf3d6000                                                                
[    2.161865] HCI device registered (hdev cf3d6000)                                        
[    2.167144] hci0 cf3d6000                                                                
[    2.169891] plat_kim_chip_enable                                                         
[    2.174652] cpuidle: using governor ladder                                               
[    2.179077] cpuidle: using governor menu                                                 
[    2.186645] usbcore: registered new interface driver usbhid                              
[    2.192504] usbhid: USB HID core driver                                                  
[    2.301605] android_work: sent uevent USB_STATE=DISCONNECTED                             
[    2.307861] logger: created 256K log 'log_main'                                          
[    2.312713] logger: created 256K log 'log_events'                                        
[    2.317718] logger: created 256K log 'log_radio'                                         
[    2.322662] logger: created 256K log 'log_system'                                        
[    2.328063] usbcore: registered new interface driver snd-usb-audio                       
[    2.335388] ALSA device list:                                                            
[    2.338531]   No soundcards found.                                                       
[    2.342102] oprofile: hardware counters not available                                    
[    2.347381] oprofile: using timer interrupt.                                             
[    2.351989] Netfilter messages via NETLINK v0.30.                                        
[    2.357025] nf_conntrack version 0.5.0 (3925 buckets, 15700 max)                         
[    2.363616] ctnetlink v0.93: registering with nfnetlink.                                 
[    2.369201] NF_TPROXY: Transparent proxy support initialized, version 4.1.0              
[    2.376495] NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.                           
[    2.382904] xt_time: kernel timezone is -0000                                            
[    2.387664] ip_tables: (C) 2000-2006 Netfilter Core Team                                 
[    2.393432] arp_tables: (C) 2002 David S. Miller                                         
[    2.398315] TCP cubic registered                                                         
[    2.401855] NET: Registered protocol family 10                                           
[    2.407226] Mobile IPv6                                                                  
[    2.409820] ip6_tables: (C) 2000-2006 Netfilter Core Team                                
[    2.415679] IPv6 over IPv4 tunneling driver                                              
[    2.420715] NET: Registered protocol family 17                                           
[    2.425384] NET: Registered protocol family 15                                           
[    2.430053] can: controller area network core (rev 20090105 abi 8)                       
[    2.436645] NET: Registered protocol family 29                                           
[    2.441314] can: raw protocol (rev 20090105)                                             
[    2.445770] can: broadcast manager protocol (rev 20090105 t)                             
[    2.451965] android_work: did not send uevent (0 0   (null))                             
[    2.458038] Bluetooth: RFCOMM TTY layer initialized                                      
[    2.463165] Bluetooth: RFCOMM socket layer initialized                                   
[    2.468505] Bluetooth: RFCOMM ver 1.11                                                   
[    2.472442] Bluetooth: BNEP (Ethernet Emulation) ver 1.3                                 
[    2.477966] Bluetooth: BNEP filters: protocol multicast                                  
[    2.483428] Bluetooth: HIDP (Human Interface Emulation) ver 1.2                          
[    2.489776] Registering the dns_resolver key type                                        
[    2.494750] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3      
[    2.502746] ThumbEE CPU extension supported.                                             
[    2.507263] mux: Failed to setup hwmod io irq -22                                        
[    2.512817] Power Management for AM33XX family                                           
[    2.517669] Trying to load am335x-pm-firmware.bin (60 secs timeout)                      
[    2.524353] Copied the M3 firmware to UMEM                                               
[    2.533111] clock: disabling unused clocks to save power                                 
[    2.540222] Detected MACID=0:18:31:e7:46:c1                                              
[    2.545745] omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (94668480)
[    2.555023] Waiting for root device /dev/mmcblk0p2...                                    
[    2.560394] android_work: did not send uevent (0 0   (null))                             
[    2.602416] android_work: sent uevent USB_STATE=CONNECTED                                
[    2.608093] android_work: sent uevent USB_STATE=DISCONNECTED                             
[    2.640686] mmc0: host does not support reading read-only switch. assuming write-enable. 
[    2.651275] mmc0: new high speed SDHC card at address e624                               
[    2.657470] mmcblk0: mmc0:e624 SU04G 3.69 GiB                                            
[    2.663635]  mmcblk0: p1 p2 p3                                                           
[    2.738220] android_work: did not send uevent (0 0   (null))                             
[    2.775024] mmc1: card claims to support voltages below the defined range. These will be.
[    2.794403] android_work: sent uevent USB_STATE=CONNECTED                                
[    2.801971] mmc1: queuing unknown CIS tuple 0x91 (3 bytes)                               
[    2.809112] mmc1: new SDIO card at address 0001                                          
[    2.992309] EXT4-fs (mmcblk0p2): recovery complete                                       
[    2.999420] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) 
[    3.007965] VFS: Mounted root (ext4 filesystem) on device 179:2.                         
[    3.014617] Freeing init memory: 252K                                                    
[    3.034515] init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj in.
[    3.120635] init: cannot open '/initlogo.rle'                                            
[    3.153411] Disabling lock debugging due to kernel taint                                 
[    3.159576] Compat-wireless backport release: compat-wireless-2011-12-05-1-g84dbe2c      
[    3.167602] Backport based on wl12xx.git v2.6.39-1328-g0890f48                           
[    3.199554] Unable to handle kernel paging request at virtual address bf03c4ea           
[    3.207153] pgd = cfa18000                                                               
[    3.209960] [bf03c4ea] *pgd=8fa57811, *pte=00000000, *ppte=00000000                      
[    3.216552] Internal error: Oops: 7 [#1]                                                 
[    3.220642] Modules linked in: compat(O)                                                 
[    3.224731] CPU: 0    Tainted: G           O  (3.2.0 #7)                                 
[    3.230285] PC is at sys_init_module+0xf9c/0x1a7c                                        
[    3.235168] LR is at 0x400                                                               
[    3.238006] pc : [<c006b6a0>]    lr : [<00000400>]    psr: 20000013                      
[    3.238006] sp : cf81def0  ip : cf802ac0  fp : cf81dfa4                                  
[    3.249969] r10: bf025784  r9 : bf025598  r8 : 0000039e                                  
[    3.255401] r7 : d08eeba8  r6 : bf0344e4  r5 : bf02558c  r4 : be913e30                   
[    3.262207] r3 : 00008006  r2 : bf0344e4  r1 : 033e00ab  r0 : bf02b34e                   
[    3.269012] Flags: nzCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user            
[    3.276458] Control: 10c5387d  Table: 8fa18019  DAC: 00000015                            
[    3.282440]                                                                              
[    3.282440] PC: 0xc006b620:                                                              
[    3.286895] b620  e2022006 e3520006 0a0000d4 e2877001 e2866010 e1570001 3affffea e59520c4
[    3.295440] b640  e3a01000 e51b306c e5858100 e0820003 e5850108 e7c21003 e3a03028 e51b7080
[    3.303985] b660  e51b205c e0237293 e5933014 e3530001 9a000014 e3a03001 e3530000 e283e01f
[    3.312561] b680  a1a0e003 e51bc074 e203101f e1a0e2ce e79cc10e e1a0113c e3110001 15952104
[    3.321105] b6a0  17d22003 e2833001 15e02001 151b205c 151b7080 e0821102 e0871181 e5911014
[    3.329650] b6c0  e1530001 3affffeb e51b0088 e1a01007 e1a02005 ebfeb1dd e250a000 ba00002c
[    3.338195] b6e0  e51b0094 e3a03000 e5907008 e5803008 e59500c0 e1500003 03026018 034c606e
[    3.346771] b700  0a000005 e3026018 e59510c8 e34c606e e0801001 e5963010 e12fff33 e59500c4
[    3.355316]                                                                              
[    3.355316] SP: 0xcf81de70:                                                              
[    3.359771] de70  ffffffff 22221000 48885100 08101111 00000262 c006b6a0 20000013 ffffffff
[    3.368316] de90  cf81dedc 0000039e cf81dfa4 cf81dea8 c0506158 c0008374 bf02b34e 033e00ab
[    3.376861] deb0  bf0344e4 00008006 be913e30 bf02558c bf0344e4 d08eeba8 0000039e bf025598
[    3.385406] ded0  bf025784 cf81dfa4 cf802ac0 cf81def0 00000400 c006b6a0 20000013 ffffffff
[    3.393981] def0  bf02558c 00000001 cfa34ac8 0000feff be913e30 d08ee888 d08ee888 00000733
[    3.402526] df10  cf81c000 bf0256ac cf81df34 d08cb000 00037410 d08eeba8 d08eea3f d08fc3d8
[    3.411071] df30  cf346000 00021784 00025374 00000000 00000000 00000025 00000026 0000001e
[    3.419647] df50  0000001a 00000018 00000000 00000000 cf81df8c cf81df70 c00a81c0 c00ab1ec
[    3.428192]                                                                              
[    3.428192] IP: 0xcf802a40:                                                              
[    3.432647] 2a40  cfa0c000 cfa0c000 cf802a48 cf802a48 cf802a50 cf802a50 0000001c 000000a4
[    3.441192] 2a60  00000000 00000000 00000000 ffff8cf6 00000001 2691093a 00e62232 6a9546d1
[    3.449737] 2a80  cf802a80 cf802a80 cfa0b000 cfa0b000 cf802a90 cf802a90 00000000 00000040
[    3.458282] 2aa0  00000001 00000000 00000000 ffff8d76 00000001 00310a6d 413e2358 0d60405c
[    3.466857] 2ac0  cf347000 cf347000 cf802ac8 cf802ac8 cf802ad0 cf802ad0 00000061 000000e9
[    3.475402] 2ae0  00000000 00000000 00000000 ffff8c66 00000001 35095068 c1087109 c05400a8
[    3.483947] 2b00  cf819000 cf819000 cf802b08 cf802b08 cf802b10 cf802b10 0000000c 0000008c
[    3.492492] 2b20  00000001 00000000 00000000 ffff8ce6 00000001 406a320c c0294313 c8b325e1
[    3.501068]                                                                              
[    3.501068] FP: 0xcf81df24:                                                              
[    3.505493] df24  d08eeba8 d08eea3f d08fc3d8 cf346000 00021784 00025374 00000000 00000000
[    3.514068] df44  00000025 00000026 0000001e 0000001a 00000018 00000000 00000000 cf81df8c
[    3.522613] df64  cf81df70 c00a81c0 c00ab1ec 00000009 c0681fa0 00000000 400e3008 ffffffff
[    3.531158] df84  be913e30 00000080 c0013648 cf81c000 00000000 00000000 cf81dfa8 c00134a0
[    3.539703] dfa4  c006a710 400e3008 ffffffff 400e3008 00037410 be913e30 4011a418 400e3008
[    3.548278] dfc4  ffffffff be913e30 00000080 00000001 00000001 00021704 00000000 4011aff0
[    3.556823] dfe4  be913e28 0000b9a3 000086cc a0000010 400e3008 e1f1c00d 803aec2c cf802b48
[    3.565368] e004  cf83f000 00000040 cf81e040 00000007 ffffffff 02e10000 00000001 00000002
[    3.573944]                                                                              
[    3.573944] R7: 0xd08eeb28:                                                              
[    3.578369] eb28  00000000 ffffffff 00000000 c08eeb34 c08eeb34 00000000 00000000 00000000
[    3.586944] eb48  00000000 ffffffff 00000000 c08eeb54 c08eeb54 00000000 00000000 00000000
[    3.595489] eb68  00000000 ffffffff 00000000 c08eeb74 c08eeb74 00000000 00000000 00000000
[    3.604034] eb88  00000000 ffffffff 00000000 c08eeb94 c08eeb94 00000000 00000000 00000000
[    3.612579] eba8  00000000 ffffffff 00000000 c08eebb4 c08eebb4 00000000 00000000 00000000
[    3.621124] ebc8  00000000 ffffffff 00000000 c08eebd4 c08eebd4 00000000 00000000 00000000
[    3.629699] ebe8  00000000 ffffffff 00000000 c08eebf4 c08eebf4 00000000 00000000 00000000
[    3.638244] ec08  00000000 ffffffff 00000000 c08eec14 c08eec14 00000000 00000000 00000000
[    3.646789] Process init (pid: 1, stack limit = 0xcf81c2f0)                              
[    3.652618] Stack: (0xcf81def0 to 0xcf81e000)                                            
[    3.657135] dee0:                                     bf02558c 00000001 cfa34ac8 0000feff
[    3.665679] df00: be913e30 d08ee888 d08ee888 00000733 cf81c000 bf0256ac cf81df34 d08cb000
[    3.674194] df20: 00037410 d08eeba8 d08eea3f d08fc3d8 cf346000 00021784 00025374 00000000
[    3.682739] df40: 00000000 00000025 00000026 0000001e 0000001a 00000018 00000000 00000000
[    3.691253] df60: cf81df8c cf81df70 c00a81c0 c00ab1ec 00000009 c0681fa0 00000000 400e3008
[    3.699768] df80: ffffffff be913e30 00000080 c0013648 cf81c000 00000000 00000000 cf81dfa8
[    3.708312] dfa0: c00134a0 c006a710 400e3008 ffffffff 400e3008 00037410 be913e30 4011a418
[    3.716827] dfc0: 400e3008 ffffffff be913e30 00000080 00000001 00000001 00021704 00000000
[    3.725372] dfe0: 4011aff0 be913e28 0000b9a3 000086cc a0000010 400e3008 e1f1c00d 803aec2c
[    3.733886] Backtrace:                                                                   
[    3.736450] [<c006a704>] (sys_init_module+0x0/0x1a7c) from [<c00134a0>] (ret_fast_syscal)
[    3.745880] Code: e79cc10e e1a0113c e3110001 15952104 (17d22003)                         
[    3.752288] ---[ end trace 16ecf17b67337997 ]---                                         
[    3.757110] Kernel panic - not syncing: Fatal exception                                  
[    3.762573] Backtrace:                                                                   
[    3.765136] [<c0016f88>] (dump_backtrace+0x0/0x110) from [<c05040b8>] (dump_stack+0x18/0)
[    3.773956]  r6:00000000 r5:cf81c000 r4:c073c8d0 r3:c0705690                             
[    3.779876] [<c05040a0>] (dump_stack+0x0/0x1c) from [<c0504128>] (panic+0x6c/0x1a0)      
[    3.787872] [<c05040bc>] (panic+0x0/0x1a0) from [<c0017284>] (die+0x134/0x2d8)           
[    3.795410]  r3:00000001 r2:00000000 r1:00000000 r0:c06003c4                             
[    3.801330]  r7:cf81dd62                                                                 
[    3.803985] [<c0017150>] (die+0x0/0x2d8) from [<c0019914>] (__do_kernel_fault+0x7c/0x8c) 
[    3.812438] [<c0019898>] (__do_kernel_fault+0x0/0x8c) from [<c0507934>] (do_page_fault+0)
[    3.821777]  r8:00010000 r7:00000007 r6:bf03c4ea r5:cfa0be00 r4:cf81dea8                 
[    3.828613] r3:cf81dea8                                                                  
[    3.831359] [<c0507890>] (do_page_fault+0x0/0x224) from [<c00083a4>] (do_DataAbort+0x3c/)
[    3.840240] [<c0008368>] (do_DataAbort+0x0/0xa0) from [<c0506158>] (__dabt_svc+0x38/0x60)
[    3.848785] Exception stack(0xcf81dea8 to 0xcf81def0)                                    
[    3.854064] dea0:                   bf02b34e 033e00ab bf0344e4 00008006 be913e30 bf02558c
[    3.862579] dec0: bf0344e4 d08eeba8 0000039e bf025598 bf025784 cf81dfa4 cf802ac0 cf81def0
[    3.871124] dee0: 00000400 c006b6a0 20000013 ffffffff                                    
[    3.876403]  r8:0000039e r7:cf81dedc r6:ffffffff r5:20000013 r4:c006b6a0                 
[    3.883422] [<c006a704>] (sys_init_module+0x0/0x1a7c) from [<c00134a0>] (ret_fast_syscal)


regards,

Akhil.