Hello team,
I would like to know whether Omap5432 EVM (GLSDK) uses ti-syslink module ? If yes, can you please locate me to the source of ti-syslink ? I would like to confirm that Omap5432 EVM is using CONFIG_RPMSG (from kernel linux-3.8.18) with AF_RPMSG (from syslink) or not !
This is a high priority query for developers who are interested to integrate "meta-ivi" (Genivi-4.0) which adds AF_BUS patch with AF_BUS sockets @ address 40 !! This should not conflict with AF_RPMSG which is also defined at same address space for Omap4 software.
https://github.com/Digilent/linux-digilent/blob/master/net/rpmsg/rpmsg_proto.c
-----------------------------------------------
-----------------------------------------------
Does this change/code holds true for Omap5432 EVM (Linux-3.8.13) ?
You inputs are highly appreciated.
Thanks & Regards.