This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AIF2 query (Problems in running example code: CPRI 4x LTE 20 Mhz 2 Link)



Hi

I am facing the following problems while running AIF2 LTE mode example for AIF2 CPRI 4x 20 Mhz 2 link on 6618 emulator board 9TMS320TCI6618 Evaluation Module with XDS560v2 Emulator- TMDXEVM6618LXE):

Scenario 1: The core 0 is in hang state when the program is loaded on CPU

 Because of the above mentioned scenario, the program cannot be run on core 0.

For other cores, sometimes, data doesnt exit Tx queue and hence the test fails. For other times, data exits Tx queue and is received on Rx, and is as expected.

 

Scenario 2: Core 0 is not in hang state and program can be run fro core 0

For all cores, data doesnt exit Tx queue and hence, the test always fails.

 

Kindly help to debug the issue.

Thanks

 

Regards

Anuj Agarwal