This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi dear forums members, we're working with Appro IPNC ref and we came across the usage of EDMA, especially in DSP domain.
As it seems, there are a max of 64 channels for a particular queue but after we've looked all over the code base (mcfw + ti section) we found only 2 *** officially *** used channels: 8 in VA_LINK and 6 in FD_LINK. Still, we believe others might be also used (we're especially interested in VA use-case flow). As we couldn't find any declared mapping of use / don't use channels we require to know the following:
1. What's the meaning of VA_LINK_EDMA3_QUEUE_ID and how it affects the usage of DMA in the system? Could I use different queue ID if I wish under DSP?
2. We saw usage of "EDMA Channel Registers for Shadow region 5" - how does it affects DSP usage? Does each CPU (M3, Cortex, DSP) have a dedicated region?
3. Are all channels shared by the entire system i.e. if some code under VPSS (M3) uses channel id 3, does it means it's locked from DSP usage? Is there some mean to know who is using what channel?
4. I read something about linked EDMA activation but couldn't figure out exactly how it should be configured. If I have 3 buffers (different ptr, different size) that I wish to move via single EDMA async event, how can I do it?
Thanks in advance,
Roei
Hi Roei,
regards,
Anand
Hi Anand, thanks for the support but is it possible to be more specific regarding what s/w or h/w block is using the EDMA channels (i.e. reserve them)?
I couldn't find any specific documentation and when I use some IDs freely, the system hangs on occasion. Parts of the system is w/o source (only libs) so how can one know what is for spare and what isn't?
Regards,
Roei
Hi Roei,
To find out the free EDMA channels,on A8 side you can call the API 'OSA_dmaOpen()' in a loop for 64 times and note the free channels it is giving out.This will be only test code.
You can use all the free EDMA channels returned by above call on any of the cores (A8,M3,DSP).
Going forward we are going to allocate EDMA channels only through above call.
regards,
Anand
Hi Anand, thanks for the fast response - just to make sure: Is this API call will tell me what is opened at the moment? If that's the case what might happen if someone is using the EDMA like I do, in an ad-hoc fashion, this might result in a timing issue i.e. maybe when I'll perform my test I will see channel id 3 (w/o loss of generality) as free but at some other point it will be used.
If I want to work in a dynamic mode, so that my algorithm will use only the currently free channel, is there a mean in DSP core (Bios6) to perform this OSA_dmaOpen query (which uses IOCTL commands)? Also, my idea cannot ensure that other modules are "nice" like me and perform this query so contention might still occur.
Regards,
Roei
Adding to my last question (which wasn't responded as of yet), I found the file /Source/ipnc_rdk/ipnc_mcfw/mcfw/src_bios6/utils/src/utils_dma_common_cfg.c that seems to hold some info regarding EDMA usage all across the system but there's a comment that suggests this is an omap device mapping:
HOST A8 - Defined in <linux kernel>\arch\arm\mach-omap2\devices.c, ti81xx_dma_rsv_chans, ti81xx_dma_rsv_slots,
but I'm working with Da-Vinci device (8148). I went further into the Linux end and looked inside:
/Source/ti_tools/ipnc_psp_04_04_00_01/kernel/arch/arm/mach-davinci/include/mach/edma.h
Somehow, this is the closest thing I've found which is related to EDMA channels usage (partial quoting):
#define DAVINCI_DMA_MCBSP_TX 2
#define DAVINCI_DMA_MCBSP_RX 3
#define DAVINCI_DMA_VPSS_HIST 4
#define DAVINCI_DMA_VPSS_H3A 5
#define DAVINCI_DMA_VPSS_PRVU 6
#define DAVINCI_DMA_VPSS_RSZ 7
#define DAVINCI_DMA_IMCOP_IMXINT 8
....
#define DAVINCI_DMA_PWM0 52
#define DAVINCI_DMA_PWM1 53
#define DAVINCI_DMA_PWM2 54
but this is also strange as channel id 6 and 8 are usage in FD, VA respectively in DSP.
I'm asking again - who's responsible in TI's support to describe what can be used and what can't... ?
Regards,
Roei
Hi Roei,
I have already replied that you need to write test code on A8 where in you call 'OSA_dmaOpen' in a loop to find out the free EDMA channels available at your disposal and you can reserve them in the kernel in 'ti81xx_dma_rsv_chans', 'ti81xx_dma_rsv_slots' structures in /arch/arm/mach-omap2/devices.c file.
'OSA_dmaOpen' takes care of reserved EDMA channels and those tied to events in the kernel while providing free channel. And in IPNC RDK ver 3.5 and below we are reserving channels 5-9 in the kernel and are used by M3 and DSP.
Going forward we are providing proper APIs on M3 and DSP to get free EDMA channels by A8.
regards,
Anand
Hi Anand, I've made the test of OSA_dmaOpen x64 calls in several places in my flow but the IDs reported aren't constant so this suggests that the channels are being somehow opened and then closed by a user. I can't really rely on such info as I need to use channels that I can be sure are mine alone to use.
Also, even if I make some OR logic and extract from several runs IDs that were never used by Linux, who can tell what VPSS and all bios6-M3 code is using?
I must say that I find it very strange there isn't some single direct map of used channels, after all, someone had to bring-up the Appro device and validate the system functionality, no?
Any thoughts of why I get non-constant free channels IDs?
To avoid confusion, this is the code I was using for finding the relevant free channels:
#define BITS64_1(n) ( 1ll << (n) )
static void PrintFreeEdmaChannels()
{
OSA_DmaChHndl dmaHndl;
int status;
status = OSA_dmaInit();
uint32 i;
uint64 dmaBit = 0;
if (status == 0)
{
for (i = 0; i < 64; i++)
{
status = OSA_dmaOpen(&dmaHndl, OSA_DMA_MODE_NORMAL, 1);
if (status != 0)
{
OSA_printf("%s:OSA_dmaOpen %u failed - %d\n", __func__, i, status);
}
else
{
// OSA_printf("%s:OSA_dmaOpen passed with ch id = %d\n", __func__, dmaHndl.chId);
dmaBit |= BITS64_1(dmaHndl.chId);
}
}
}
else
{
OSA_printf("%s:OSA_dmaInit failed - %d\n", __func__, status);
}
for (i = 0; i < 64; i++)
{
if ((BITS64_1(i) & dmaBit) == 0)
{
OSA_printf("OSA_dmaOpen free for bios6 = %u\n", i);
}
}
}
Regards,
Roei
Hi Roei,
Static allocation of EDMA channels is done in the kernel using the following info:
The remainig channels are free and can be dynamically allocated to the user.
When we call OSA_dmaOpen() API a free available channel is given to you and is marked as not available.
So if you call the loop multiple times then you will surely get different values.
So the thumb rule for using the EDMA channels is:
This is how we have been using EDMA channels on M3 and DSP.
regards,
Anand
First, Anand, let me say thanks for your quick support. I feel like I understand most of the issues I've queried but the M3 size is still a bit vague. The IPNC Appro device is a demo kit with many features. What ensures me under, let's say, the video / capture / display that they don't use EDMA channels from this free list? I looked freely over the code and couldn't find some link / ti_tools code that is using directly the EDMA - does this means that I can use all the free ones w/o fearing I will have some conflict?
If that's the case then I'm done else it would be nice to have some mean (code, contact person, doc) that state the M3 used channels. What about the OSD windows, I would think those also use DMA for fast block copy...
Regards,
Roei