Hi,
I Used the Master tool (TwinCAT) to run the slave(ICE) and the slave is SYS/BIOS SDK 1.0.0.7 of AM335x ICE .
if I set the TwinCAT run in DC mode and Disable Sync1 signal , the slave's state of infoData parameter will be 0x52, and the ERR led light.
the error message in TwinCAT is:
0x___2 = Slave in 'PREOP' state
0x001_ = Slave signals error
0x004_ = Initialization error occurred