Hello,
I have a problem with the POWER UP for Sitara.
--------------USE--------------------------
I use AM3357 with:
DDR2 - 2 banks ( 2 x 256Mb)
NAND Flash (256Mb)
USB
Ethernet....
For Power chip I use : TPS65910AA1RSL
-------------Schematic and PCB-----------------------
I connected the power supply rails, as recommendations: http://www.ti.com/lit/ug/swcu093c/swcu093c.pdf page:6
My reference design is ICE : http://www.ti.com/tool/tmdxice3359#1 and IDK : http://www.ti.com/tool/tmdxidk3359#0 ( for 2 banks DDR2 memory)
VDDIO Rail of TPS65910AA1RSL is 3,3V
The BOOT Sequence is: NAND / NAND I2C / SPI0 / EMAC1
-----------------The Problem----------------------------------------
My problem occurs in the following:
When I turn on the power, see how quartz (24mhz) works, how the Sitara searches for boot device to Ethernet ... and so on.
but Power Rail "VIO" who responsible for the supply of DDR2, activates defense. After disconnecting the power supply, I find that VIO to GND is short. (I want to note that before turning on the Power for the first time, betweеn VIO and GND no present the short). The PCB is 6 layer stack with Planes Power and GND and Routing by recomendation of Datasheet of Texas Instruments. I want to note that even with a burned bus "VIO" , processor running with no problems
This phenomenon with VIO Rail appears for all my test PCB's. For some of the boards I pulled DDR2 memory banks, and found that the memory is ОК. (not burned)
probably the problem is around Sitara
Suggest me where to look for problems.
Best Regards