This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 PCIe IpcFramesOutLink

Hi

 I want to capture video from PCIe,In my usecase,I use  the ipcFramesOutHost Link and ipcFramesInVpss link ,and I invoke Vsys_allocBuf() to allocate shard region firstly,then,pass it to  ipcFramesOut_putFullFrames.

IpcFramesOutLink_getEmptyVideoFrames---->get data from PCIe----->IpcFramesOutLink_putFullVideoFramesIn

In my program,we connect and disconnect PCIe dynamically,the issue is that when I connect 4 times ,the M3VPSS will down with the infomation:

218030:!!!SLAVE CORE [VPSS-M3] DOWN!!!
SystemLink_copySlaveCoreExceptionContext:146
mmap of [0xbe9e0000:36864]
mmap virt addresss:0x413b7000
munmap of [0x413b7000:36864]
SystemLink_copySlaveCoreExceptionContext:153
 [m3vpss ]  256337: Assertion @ Line: 2099 in links_m3vpss/avsync/avsync_m3vpss.c: freeFrameList->numFrames < UTILS_ARRAYSIZE(freeFrameList->frames) : failed !!!
218030:!!!SLAVE CORE [VPSS-M3] DOWN!!!
SystemLink_copySlaveCoreExceptionContext:146
mmap of [0xbe9e0000:36864]
mmap virt addresss:0x413b7000
munmap of [0x413b7000:36864]
SystemLink_copySlaveCoreExceptionContext:153
 [m3vpss ]  256337: Assertion @ Line: 2099 in links_m3vpss/avsync/avsync_m3vpss.c: freeFrameList->numFrames < UTILS_ARRAYSIZE(freeFrameList->frames) : failed !!!

I want to know  the reason lead to this issue.

Looking forward to your reply.

  • The assert indicates the number of video frames in SwMs exceeds  64 frames for a single channel. Maintain a counter in your application and check the number of frame sent for a channel by ipcFramesOutLink_putFullVideoFrames but not received by ipcFramesOutLink_getEmptyVideoFrames.Also attach your application file which does frame exchange with ipcFramesOut link.