Other Parts Discussed in Thread: TMS320C5515
Hello,
I am developing a program with TMS320C5515 EVM and CCS 4.1. In that board, the codec AIC3204 is connected to I2S2 bus, and J13 has I2S1 outputs. I have connected I2S1 SCK, WS, SI and SO to a peripheral. What I want to do is play audio through the peripheral by using DMA controller. For that purpose, I defined a sine of 1KHz sampled at 48KHz, and I used DMA controller 3 with channel 0 and channel 1 for Left and Right (Stereo Mode). However, I can't reproduce the audio, and I don't know what I am doing bad.
Moreover, I would know If there are any example or you explain me, how can I do to take the input of Stereo in 1 of the board (Codec connected to I2S2) and route the signal to the peripheral.
Thank you!
Albert Torne