This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x pin mux power confict

Hello

Is below IO power violation acceptable ?

 I'm using 8bit data width 1.8v NAND flash, the selected IO set is 50 and after de selecting unused signals interface include

csn0,advn_ale,oen_ren,wen,beon_ale and 8bit data powered from VDDSHV1=1.8V and  wait0 (gpio0(30) powered from  VDDSHV3=3.3V

I used a 1.8v to 3.3V level shifter for wait0 signal is this acceptable ?

Yoni