Other Parts Discussed in Thread: TPS65910, DA8XX, TMP275
Hi, I am trying to boot with a multi image file that was generated with mkimage. The uboot decompress the file and find the kernel, but is not find the filesystem. How can I fix the ramdisk address in ram to call bootm in right way?
- Attached is the environment variables.
- command line used to mkimage: mkimage -A arm -T multi -C gzip -a 0 -e 0 -n 'test multifile' -d vmlinux:ramdisk.gz uMulti
- Bellow is the log:
## Booting kernel from Legacy Image at 80007fc0 ...
Image Name: test multifile
Image Type: ARM Linux Multi-File Image (gzip compressed)
Data Size: 14018554 Bytes = 13.4 MiB
Load Address: 00000000
Entry Point: 00000000
Contents:
Image 0: 3207239 Bytes = 3.1 MiB
Image 1: 10811302 Bytes = 10.3 MiB
Verifying Checksum ... OK
## Loading init Ramdisk from Legacy Image at 80007fc0 ...
Image Name: test multifile
Image Type: ARM Linux Multi-File Image (gzip compressed)
Data Size: 14018554 Bytes = 13.4 MiB
Load Address: 00000000
Entry Point: 00000000
Contents:
Image 0: 3207239 Bytes = 3.1 MiB
Image 1: 10811302 Bytes = 10.3 MiB
Verifying Checksum ... OK
No Linux ARM Ramdisk Image
Ramdisk image is corrupt or invalid
U-Boot# printenv
baudrate=115200
bootargs=console=ttyO0,115200n8
bootargs_defaults=setenv bootargs console=${console} ${optargs}
bootcmd=if mmc rescan ${mmcdev}; then echo SD/MMC found on device ${mmcdev};if run loadbootenv; then echo Loaded environment from ${bootenv};r
un importbootenv;fi;if test -n $uenvcmd; then echo Running uenvcmd ...;run uenvcmd;fi;if run loaduimagefat; then run mmcboot;elif run loaduima
ge; then run mmcboot;else echo Cound not find ${bootfile} ;fi;else run nandboot;fi;
bootdelay=3
bootenv=uEnv.txt
bootfile=uImage
bootm=0x00000000 0x80007fc0
console=ttyO0,115200n8
dfu_alt_info=SPL part 0 1;SPL.backup1 part 0 2;SPL.backup2 part 0 3;SPL.backup3 part 0 4;u-boot part 0 5;kernel part 0 7;rootfs part 0 8
ethact=cpsw
ethaddr=00:18:31:e0:9a:d1
fdtaddr=0x80F80000
filesize=D5E83A
importbootenv=echo Importing environment from mmc ...; env import -t $loadaddr $filesize
ip_method=none
kloadaddr=0x80007fc0
loadaddr=0x80200000
loadbootenv=fatload mmc ${mmcdev} ${loadaddr} ${bootenv}
loadramdisk=fatload mmc ${mmcdev} ${rdaddr} ramdisk.gz
loaduimage=ext2load mmc ${mmcdev}:2 ${kloadaddr} /boot/${bootfile}
loaduimagefat=fatload mmc ${mmcdev} ${kloadaddr} ${bootfile}
mmcargs=run bootargs_defaults;setenv bootargs ${bootargs} root=${mmcroot} rootfstype=${mmcrootfstype} ip=${ip_method}
mmcboot=echo Booting from mmc ...; run mmcargs; bootm ${kloadaddr}
mmcdev=0
mmcroot=/dev/mmcblk0p2 rw
mmcrootfstype=ext2 rootwait
mtddevname=SPL
mtddevnum=0
mtdids=nand0=omap2-nand.0
mtdparts=mtdparts=omap2-nand.0:128k(SPL),128k(SPL.backup1),128k(SPL.backup2),128k(SPL.backup3),1920k(u-boot),128k(u-boot-env),5m(kernel),12441
6k(fs1),124416k(fs2),-(safe_area)
nand_erasesize=20000
nand_oobsize=40
nand_writesize=800
nandargs=run bootargs_defaults;setenv bootargs ${bootargs} root=${nandroot} noinitrd rootfstype=${nandrootfstype} ip=${ip_method}
nandboot=echo Booting from nand ...; run nandargs; nand read.i ${kloadaddr} ${nandsrcaddr} ${nandimgsize}; bootm ${kloadaddr}
nandimgsize=0x1000000
nandroot=ubi0:rootfs rw ubi.mtd=7,2048 noinitrd
nandrootfstype=ubifs rootwait=1
nandsrcaddr=0x780000
netargs=run bootargs_defaults;setenv bootargs ${bootargs} root=/dev/nfs nfsroot=${serverip}:${rootpath},${nfsopts} rw ip=dhcp
netboot=echo Booting from network ...; setenv autoload no; dhcp; tftp ${kloadaddr} ${bootfile}; run netargs; bootm ${kloadaddr}
nfsopts=nolock
partition=nand0,0
ramargs=setenv bootargs console=ttyO0,115200n8 root=/dev/ram0 rw ramdisk_size=65536 initrd=${rdaddr},64M rootfstype=ext2
ramboot=echo Booting from ramdisk ...; run ramargs; bootm 0x80200000
ramroot=/dev/ram0 rw ramdisk_size=65536 initrd=0x81000000,64M
ramrootfstype=ramdisk
rdaddr=84207239
rootpath=/export/rootfs
selected_img=1
spiargs=run bootargs_defaults;setenv bootargs ${bootargs} rootfstype=${spirootfstype} ip=${ip_method}
spiboot=echo Booting from spi ...; run spiargs; sf probe ${spibusno}:0; sf read ${kloadaddr} ${spisrcaddr} ${spiimgsize}; bootm ${kloadaddr}
spibusno=0
spiimgsize=0x362000
spiroot=/dev/mtdblock4 rw
spirootfstype=jffs2
spisrcaddr=0x80000
static_ip=${ipaddr}:${serverip}:${gatewayip}:${netmask}:${hostname}::off
stderr=serial
stdin=serial
stdout=serial
usbnet_devaddr=00:18:31:e0:9a:d1
ver=U-Boot 2012.10 (Dec 16 2012 - 13:54:10)
Environment size: 3358/131068 bytes
thank you for any help