We use DVR RDK 03.00.00.00 / DM8168 / Udworks platform
I try to use EMAC Boot to Flash Uboot.
I followed the instructions in DVR RDK V3.0 Installation Guide.
After setup Tftp32 I was looking for u-boot.bin in the
pre_build_binary folder (I also searched in the other versions > 1.9 of DVR DRK).
But this binary "u-boot.bin" seems only to be in version 02.80.0.10.
I used this bootfile but without success. I can not boot via Tftp32.
Is it possible to get or to compile this bootfile ?