This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

encoder question

rdk3.0

did you know the range of bit-rate for h264 codec?

did you know the range of frame-rate for h264 codec?

  • after checking H264_Encoder_HDVICP2_UserGuide.pdf under ti_tools\codecs\REL.500.V.H264AVC.E.IVAHD.02.00.02.02\500.V.H264AVC.E.IVAHD.02.00\IVAHD_001\Docs

    What is the maximum bit rate supported?

    Maximum bit rate depends upon the level setting. This version supports the maximum bit rate of 50 mbps (Base Line and Main profile Level 4.2) and 62.5 mbps (High Profile Level 4.2) for 30 fps case. To achieve the real time performance with CABAC bit rate should be less than 25 Mbps for 30fps case