hi.
development Environment.
- Code Composer Studio Version: 5.4.0.00091
- sdk : AM335x SYSBIOS Industrial SDK 01.00.00.08
- target : AM335x IDK( EtherCAT Slave )
Building Full Feature EtherCAT Application. I'm test complete.
However. Generating AM335x EtherCAT sources using Beckhoff SSC Tool problem occurred.
in SDK user guide :
1. Save the project >> No problem.
2. Click "Project->Create new Salve Files" - This generate the ETherCAT Source files for TI AM335x device. >> No problem.( Generate source files )
3. Now apply the patch file on top of the generated source file. On successful patch process, the source now includes all TI specific changes and can be used to build a full featured EtherCAT application. >> Applying a patch file problem.
CMD window message:
|
C:\software\lasted\patch-2.5.9-7-bin\bin>patch.exe -i C:\software\lasted\TIAM335 x_SSC_xml_patch_1_7\TI_ESC_Patch.patch -d C:\software\lasted\TIAM335x_SSC_xml_pa tch_1_7\Src patching file bootmode.c patching file ecat_def.h patching file ecatappl.c patching file ecateoe.c patching file ecatslv.c patching file ecatslv.h patching file eoeappl.c patching file tiescappl.c Hunk #1 FAILED at 87. Hunk #2 FAILED at 734. Hunk #3 FAILED at 753. 3 out of 3 hunks FAILED -- saving rejects to file tiescappl.c.rej |
bulid link error occurred.
However "SSC Tool" if not used, build succesed.
|
C:\software\lasted\patch-2.5.9-7-bin\bin>patch.exe -i C:\ti\am335x_sysbios_ind_s dk_1.0.0.8\sdk\protocols\ethercat_slave\ecat_appl\patch\TI_ECAT.patch -d C:\soft ware\lasted\SSC_V5i01\SlaveFiles\src patching file bootmode.c patching file cia402appl.c patching file coeappl.c patching file ecat_def.h patching file ecatappl.c patching file ecateoe.c patching file ecatslv.c patching file ecatslv.h patching file eoeappl.c patching file EtherCATSampleLibrary.h patching file sdoserv.c |
I do not know the cause of the problem.
thank you.
Chae.