Other Parts Discussed in Thread: OMAP-L137
Hi everyone.
I'm using ubuntu on vmware workstation and using hyperterminal. My board is OMAP-L137 revision I.
Net setting of vmware is bridge, on Ubuntu is manual, on u-boot is static ip. I don't have a router, so I use a Ethernet cable to connect the PC and EVM directly.
The cable is not crossover. I also have atftp, tftp-hpa on my Ubuntu and they are runing, all firewalls are shut down.
My Ubuntu host IP (using ifconig) is 192.168.91.10 and Win 7 IP is 192.168.91.1
but when I enter "ping 192.168.91.10" in u-boot, it shows:
ping failed; host 192.168.91.10 is not alive. Even ping 127.0.0.1 or "setenv" a ipaddr and ping it also show the same.
When try tftp, it just keep loadding:"T T T T T..." and retry. VMWare and Win 7 command prompt can ping themselves.
I searched some similar threads, but couldn't find the solution. It seems most cases working with dhcp are fine.
Please help me with it, thank you!
Ming