Other Parts Discussed in Thread: CCSTUDIO
Hi, I'm trying to upgrade from TI-RTOS 1.01 to TI-RTOS 1.10 (the current release). I downloaded and installed the 1.10 package, and it indicates that I'm missing a dependency. The error message is below:
Operation details
Your original request has been modified.
"TI-RTOS (IDE Client)" is already installed, so an update will be performed instead.
"RTSC/XDCtools (IDE Client)" is already installed, so an update will be performed instead.
Cannot complete the install because one or more required items could not be found.
Software being installed: RTSC/XDCtools (IDE Client) 3.25.0.48 (org.eclipse.rtsc.xdctools.product.ui.feature.group 3.25.0.48)
Missing requirement: Graphical Properties UI 1.0.0.201303121621 (com.ti.ccstudio.grace.ui 1.0.0.201303121621) requires 'bundle com.ti.browser 1.0.0' but it could not be found
Cannot satisfy dependency:
From: RTSC/XDCtools (IDE Client) 3.25.0.48 (org.eclipse.rtsc.xdctools.product.ui.feature.group 3.25.0.48)
To: com.ti.ccstudio.grace.ui [1.0.0.201303121621]
I went out and found Grace 1.0, which seems to be what this is asking for, and I installed it. Unfortunately it did not recognize it as helping to meet this dependency. Two questions now come up:
1. What do I need to install to meet this dependency, and
2. Why isn't it already included in the RTOS package, or mentioned on the RTOS page where I get the package? There's no link there to dependencies, nor any indication that there are any.