Hi, is just that i'm trying to change the resolution from the panel-generic display driver to handle separetly resolutions in DVI output and the second parallel display option in Pandaboard, but apparently both displays are being handled by the same driver, is it possible to handle it with different drivers and have different resolutions?, and if not, how do i turn off one of the displays (DVI or LCD) and leave the other one on? i tried but both get turned off. (i'm using android 4.0 with kernel 3.0.8).
Thanks in advanced.