Hi,
I want to reset ARM CorePac while c66x CorePac is alive In EVM.
It is explained that ARM can reset each c66x CorePac using MPM. How about the reverse case if c66x CorePac can detect ARM CorePac hang?
In ARM CorePac User Guide (spruhj4.pdf), It is stated that "The only recovery mechanism is therefore likely to be a system-level global warm reset, since ARM CorePac full power doen and disconnect sequence can not be complete in the midst of a CPU hang condition."
1) Can c66x CorePac power down and up an entire ARM CorePac?
2) Can ARM CorePac power down and up an entire ARM CorePac if it is in normal operation mode?
3) If an entire ARM CorePac is power down and up, then where is the starting point when ARM/c66x CorePac boot mode?