Hi,
I am using DM368 IPNC with RDK version 5.1.0.
I wanted to know whether the following settings are supported in the existing RDK:
1.Ipv6 settings
2.Speed(10/100 Mbps) and duplex settings(full duplex/half duplex)
If these settings are possible, which file in RDK i should look into.
Thanks in advance for the help.
-Kamala N.