Hello,
I am trying to program TCP2, but there are always some errors in the output. Furthermore, The greater number of iterations, the greater number of wrong bits in the output. The best result that I have got is around 20 error bits over 2000 bits, for only one iteration.
Maybe, this problem is related to the following sentence:
"Also note that interleaved parities must be de-interleaved prior to being sent to TCP2." on page 22, SPRU973
I do not understand the meaning of that sentence and, therefore, I do not how to implement an algorithm for that.
Where could I find additional information or any explanation?
Thank you in advance,
David.