This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[i2c arbitration error] when using 8bit i2c addr and 16bit data recv



 

Hi,

we are using 8bit non-stand i2c device for LED control .(our env is ti8167)

our LED device is RTL8231 and it's i2c is like belows image. we using 8bit i2c addr and read 16bit data.  

i changed i2c-omap.c

*
 * TI OMAP I2C master mode driver
 *
 * Copyright (C) 2003 MontaVista Software, Inc.
 * Copyright (C) 2005 Nokia Corporation
 * Copyright (C) 2004 - 2007 Texas Instruments.
 *
 * Originally written by MontaVista Software, Inc.
 * Additional contributions by:
 *	Tony Lindgren <tony@atomide.com>
 *	Imre Deak <imre.deak@nokia.com>
 *	Juha Yrjölä <juha.yrjola@solidboot.com>
 *	Syed Khasim <x0khasim@ti.com>
 *	Nishant Menon <nm@ti.com>
 *
 * This program is free software; you can redistribute it and/or modify
 * it under the terms of the GNU General Public License as published by
 * the Free Software Foundation; either version 2 of the License, or
 * (at your option) any later version.
 *
 * This program is distributed in the hope that it will be useful,
 * but WITHOUT ANY WARRANTY; without even the implied warranty of
 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
 * GNU General Public License for more details.
 *
 * You should have received a copy of the GNU General Public License
 * along with this program; if not, write to the Free Software
 * Foundation, Inc., 675 Mass Ave, Cambridge, MA 02139, USA.
 */

#include <linux/module.h>
#include <linux/delay.h>
#include <linux/i2c.h>
#include <linux/err.h>
#include <linux/interrupt.h>
#include <linux/completion.h>
#include <linux/platform_device.h>
#include <linux/clk.h>
#include <linux/io.h>
#include <linux/slab.h>
#include <linux/i2c-omap.h>
#include <linux/pm_runtime.h>

/* I2C controller revisions */
#define OMAP_I2C_REV_2			0x20

/* I2C controller revisions present on specific hardware */
#define OMAP_I2C_REV_ON_2430		0x36
#define OMAP_I2C_REV_ON_3430		0x3C
#define OMAP_I2C_REV_ON_4430		0x40

/* timeout waiting for the controller to respond */
#define OMAP_I2C_TIMEOUT (msecs_to_jiffies(1000))

/* For OMAP3 I2C_IV has changed to I2C_WE (wakeup enable) */
enum {
	OMAP_I2C_REV_REG = 0,
	OMAP_I2C_IE_REG,
	OMAP_I2C_STAT_REG,
	OMAP_I2C_IV_REG,
	OMAP_I2C_WE_REG,
	OMAP_I2C_SYSS_REG,
	OMAP_I2C_BUF_REG,
	OMAP_I2C_CNT_REG,
	OMAP_I2C_DATA_REG,
	OMAP_I2C_SYSC_REG,
	OMAP_I2C_CON_REG,
	OMAP_I2C_OA_REG,
	OMAP_I2C_SA_REG,
	OMAP_I2C_PSC_REG,
	OMAP_I2C_SCLL_REG,
	OMAP_I2C_SCLH_REG,
	OMAP_I2C_SYSTEST_REG,
	OMAP_I2C_BUFSTAT_REG,
	OMAP_I2C_REVNB_LO,
	OMAP_I2C_REVNB_HI,
	OMAP_I2C_IRQSTATUS_RAW,
	OMAP_I2C_IRQENABLE_SET,
	OMAP_I2C_IRQENABLE_CLR,
};

/* I2C Interrupt Enable Register (OMAP_I2C_IE): */
#define OMAP_I2C_IE_XDR		(1 << 14)	/* TX Buffer drain int enable */
#define OMAP_I2C_IE_RDR		(1 << 13)	/* RX Buffer drain int enable */
#define OMAP_I2C_IE_XRDY	(1 << 4)	/* TX data ready int enable */
#define OMAP_I2C_IE_RRDY	(1 << 3)	/* RX data ready int enable */
#define OMAP_I2C_IE_ARDY	(1 << 2)	/* Access ready int enable */
#define OMAP_I2C_IE_NACK	(1 << 1)	/* No ack interrupt enable */
#define OMAP_I2C_IE_AL		(1 << 0)	/* Arbitration lost int ena */

/* I2C Status Register (OMAP_I2C_STAT): */
#define OMAP_I2C_STAT_XDR	(1 << 14)	/* TX Buffer draining */
#define OMAP_I2C_STAT_RDR	(1 << 13)	/* RX Buffer draining */
#define OMAP_I2C_STAT_BB	(1 << 12)	/* Bus busy */
#define OMAP_I2C_STAT_ROVR	(1 << 11)	/* Receive overrun */
#define OMAP_I2C_STAT_XUDF	(1 << 10)	/* Transmit underflow */
#define OMAP_I2C_STAT_AAS	(1 << 9)	/* Address as slave */
#define OMAP_I2C_STAT_AD0	(1 << 8)	/* Address zero */
#define OMAP_I2C_STAT_XRDY	(1 << 4)	/* Transmit data ready */
#define OMAP_I2C_STAT_RRDY	(1 << 3)	/* Receive data ready */
#define OMAP_I2C_STAT_ARDY	(1 << 2)	/* Register access ready */
#define OMAP_I2C_STAT_NACK	(1 << 1)	/* No ack interrupt enable */
#define OMAP_I2C_STAT_AL	(1 << 0)	/* Arbitration lost int ena */

/* I2C WE wakeup enable register */
#define OMAP_I2C_WE_XDR_WE	(1 << 14)	/* TX drain wakup */
#define OMAP_I2C_WE_RDR_WE	(1 << 13)	/* RX drain wakeup */
#define OMAP_I2C_WE_AAS_WE	(1 << 9)	/* Address as slave wakeup*/
#define OMAP_I2C_WE_BF_WE	(1 << 8)	/* Bus free wakeup */
#define OMAP_I2C_WE_STC_WE	(1 << 6)	/* Start condition wakeup */
#define OMAP_I2C_WE_GC_WE	(1 << 5)	/* General call wakeup */
#define OMAP_I2C_WE_DRDY_WE	(1 << 3)	/* TX/RX data ready wakeup */
#define OMAP_I2C_WE_ARDY_WE	(1 << 2)	/* Reg access ready wakeup */
#define OMAP_I2C_WE_NACK_WE	(1 << 1)	/* No acknowledgment wakeup */
#define OMAP_I2C_WE_AL_WE	(1 << 0)	/* Arbitration lost wakeup */

#define OMAP_I2C_WE_ALL		(OMAP_I2C_WE_XDR_WE | OMAP_I2C_WE_RDR_WE | \
				OMAP_I2C_WE_AAS_WE | OMAP_I2C_WE_BF_WE | \
				OMAP_I2C_WE_STC_WE | OMAP_I2C_WE_GC_WE | \
				OMAP_I2C_WE_DRDY_WE | OMAP_I2C_WE_ARDY_WE | \
				OMAP_I2C_WE_NACK_WE | OMAP_I2C_WE_AL_WE)

/* I2C Buffer Configuration Register (OMAP_I2C_BUF): */
#define OMAP_I2C_BUF_RDMA_EN	(1 << 15)	/* RX DMA channel enable */
#define OMAP_I2C_BUF_RXFIF_CLR	(1 << 14)	/* RX FIFO Clear */
#define OMAP_I2C_BUF_XDMA_EN	(1 << 7)	/* TX DMA channel enable */
#define OMAP_I2C_BUF_TXFIF_CLR	(1 << 6)	/* TX FIFO Clear */

/* I2C Configuration Register (OMAP_I2C_CON): */
#define OMAP_I2C_CON_EN		(1 << 15)	/* I2C module enable */
#define OMAP_I2C_CON_BE		(1 << 14)	/* Big endian mode */
#define OMAP_I2C_CON_OPMODE_HS	(1 << 12)	/* High Speed support */
#define OMAP_I2C_CON_STB	(1 << 11)	/* Start byte mode (master) */
#define OMAP_I2C_CON_MST	(1 << 10)	/* Master/slave mode */
#define OMAP_I2C_CON_TRX	(1 << 9)	/* TX/RX mode (master only) */
#define OMAP_I2C_CON_XA		(1 << 8)	/* Expand address */
#define OMAP_I2C_CON_RM		(1 << 2)	/* Repeat mode (master only) */
#define OMAP_I2C_CON_STP	(1 << 1)	/* Stop cond (master only) */
#define OMAP_I2C_CON_STT	(1 << 0)	/* Start condition (master) */

/* I2C SCL time value when Master */
#define OMAP_I2C_SCLL_HSSCLL	8
#define OMAP_I2C_SCLH_HSSCLH	8

/* I2C System Test Register (OMAP_I2C_SYSTEST): */
#ifdef DEBUG
#define OMAP_I2C_SYSTEST_ST_EN		(1 << 15)	/* System test enable */
#define OMAP_I2C_SYSTEST_FREE		(1 << 14)	/* Free running mode */
#define OMAP_I2C_SYSTEST_TMODE_MASK	(3 << 12)	/* Test mode select */
#define OMAP_I2C_SYSTEST_TMODE_SHIFT	(12)		/* Test mode select */
#define OMAP_I2C_SYSTEST_SCL_I		(1 << 3)	/* SCL line sense in */
#define OMAP_I2C_SYSTEST_SCL_O		(1 << 2)	/* SCL line drive out */
#define OMAP_I2C_SYSTEST_SDA_I		(1 << 1)	/* SDA line sense in */
#define OMAP_I2C_SYSTEST_SDA_O		(1 << 0)	/* SDA line drive out */
#endif

/* OCP_SYSSTATUS bit definitions */
#define SYSS_RESETDONE_MASK		(1 << 0)

/* OCP_SYSCONFIG bit definitions */
#define SYSC_CLOCKACTIVITY_MASK		(0x3 << 8)
#define SYSC_SIDLEMODE_MASK		(0x3 << 3)
#define SYSC_ENAWAKEUP_MASK		(1 << 2)
#define SYSC_SOFTRESET_MASK		(1 << 1)
#define SYSC_AUTOIDLE_MASK		(1 << 0)

#define SYSC_IDLEMODE_SMART		0x2
#define SYSC_CLOCKACTIVITY_FCLK		0x2

/* Errata definitions */
#define I2C_OMAP_ERRATA_I207		(1 << 0)
#define I2C_OMAP3_1P153			(1 << 1)

struct omap_i2c_dev {
	struct device		*dev;
	void __iomem		*base;		/* virtual */
	int			irq;
	int			reg_shift;      /* bit shift for I2C register addresses */
	struct completion	cmd_complete;
	struct resource		*ioarea;
	u32			latency;	/* maximum mpu wkup latency */
	void			(*set_mpu_wkup_lat)(struct device *dev,
						    long latency);
	u32			speed;		/* Speed of bus in Khz */
	u16			cmd_err;
	u8			*buf;
	u8			*regs;
	size_t			buf_len;
	struct i2c_adapter	adapter;
	u8			fifo_size;	/* use as flag and value
						 * fifo_size==0 implies no fifo
						 * if set, should be trsh+1
						 */
	u8			rev;
	unsigned		b_hw:1;		/* bad h/w fixes */
	unsigned		idle:1;
	u16			iestate;	/* Saved interrupt register */
	u16			pscstate;
	u16			scllstate;
	u16			sclhstate;
	u16			bufstate;
	u16			syscstate;
	u16			westate;
	u16			errata;
};

const static u8 reg_map[] = {
	[OMAP_I2C_REV_REG] = 0x00,
	[OMAP_I2C_IE_REG] = 0x01,
	[OMAP_I2C_STAT_REG] = 0x02,
	[OMAP_I2C_IV_REG] = 0x03,
	[OMAP_I2C_WE_REG] = 0x03,
	[OMAP_I2C_SYSS_REG] = 0x04,
	[OMAP_I2C_BUF_REG] = 0x05,
	[OMAP_I2C_CNT_REG] = 0x06,
	[OMAP_I2C_DATA_REG] = 0x07,
	[OMAP_I2C_SYSC_REG] = 0x08,
	[OMAP_I2C_CON_REG] = 0x09,
	[OMAP_I2C_OA_REG] = 0x0a,
	[OMAP_I2C_SA_REG] = 0x0b,
	[OMAP_I2C_PSC_REG] = 0x0c,
	[OMAP_I2C_SCLL_REG] = 0x0d,
	[OMAP_I2C_SCLH_REG] = 0x0e,
	[OMAP_I2C_SYSTEST_REG] = 0x0f,
	[OMAP_I2C_BUFSTAT_REG] = 0x10,
};

const static u8 omap4_reg_map[] = {
	[OMAP_I2C_REV_REG] = 0x04,
	[OMAP_I2C_IE_REG] = 0x2c,
	[OMAP_I2C_STAT_REG] = 0x28,
	[OMAP_I2C_IV_REG] = 0x34,
	[OMAP_I2C_WE_REG] = 0x34,
	[OMAP_I2C_SYSS_REG] = 0x90,
	[OMAP_I2C_BUF_REG] = 0x94,
	[OMAP_I2C_CNT_REG] = 0x98,
	[OMAP_I2C_DATA_REG] = 0x9c,
	[OMAP_I2C_SYSC_REG] = 0x20,
	[OMAP_I2C_CON_REG] = 0xa4,
	[OMAP_I2C_OA_REG] = 0xa8,
	[OMAP_I2C_SA_REG] = 0xac,
	[OMAP_I2C_PSC_REG] = 0xb0,
	[OMAP_I2C_SCLL_REG] = 0xb4,
	[OMAP_I2C_SCLH_REG] = 0xb8,
	[OMAP_I2C_SYSTEST_REG] = 0xbC,
	[OMAP_I2C_BUFSTAT_REG] = 0xc0,
	[OMAP_I2C_REVNB_LO] = 0x00,
	[OMAP_I2C_REVNB_HI] = 0x04,
	[OMAP_I2C_IRQSTATUS_RAW] = 0x24,
	[OMAP_I2C_IRQENABLE_SET] = 0x2c,
	[OMAP_I2C_IRQENABLE_CLR] = 0x30,
};

static inline void omap_i2c_write_reg(struct omap_i2c_dev *i2c_dev,
				      int reg, u16 val)
{
	__raw_writew(val, i2c_dev->base +
			(i2c_dev->regs[reg] << i2c_dev->reg_shift));
}

static inline u16 omap_i2c_read_reg(struct omap_i2c_dev *i2c_dev, int reg)
{
	return __raw_readw(i2c_dev->base +
				(i2c_dev->regs[reg] << i2c_dev->reg_shift));
}

static void omap_i2c_unidle(struct omap_i2c_dev *dev)
{
	struct platform_device *pdev;
	struct omap_i2c_bus_platform_data *pdata;

	WARN_ON(!dev->idle);

	pdev = to_platform_device(dev->dev);
	pdata = pdev->dev.platform_data;

	pm_runtime_get_sync(&pdev->dev);

	if (cpu_is_omap34xx()) {
		omap_i2c_write_reg(dev, OMAP_I2C_CON_REG, 0);
		omap_i2c_write_reg(dev, OMAP_I2C_PSC_REG, dev->pscstate);
		omap_i2c_write_reg(dev, OMAP_I2C_SCLL_REG, dev->scllstate);
		omap_i2c_write_reg(dev, OMAP_I2C_SCLH_REG, dev->sclhstate);
		omap_i2c_write_reg(dev, OMAP_I2C_BUF_REG, dev->bufstate);
		omap_i2c_write_reg(dev, OMAP_I2C_SYSC_REG, dev->syscstate);
		omap_i2c_write_reg(dev, OMAP_I2C_WE_REG, dev->westate);
		omap_i2c_write_reg(dev, OMAP_I2C_CON_REG, OMAP_I2C_CON_EN);
	}
	dev->idle = 0;

	/*
	 * Don't write to this register if the IE state is 0 as it can
	 * cause deadlock.
	 */
	if (dev->iestate)
		omap_i2c_write_reg(dev, OMAP_I2C_IE_REG, dev->iestate);
}

static void omap_i2c_idle(struct omap_i2c_dev *dev)
{
	struct platform_device *pdev;
	struct omap_i2c_bus_platform_data *pdata;
	u16 iv;

	WARN_ON(dev->idle);

	pdev = to_platform_device(dev->dev);
	pdata = pdev->dev.platform_data;

	dev->iestate = omap_i2c_read_reg(dev, OMAP_I2C_IE_REG);
	if (dev->rev >= OMAP_I2C_REV_ON_4430)
		omap_i2c_write_reg(dev, OMAP_I2C_IRQENABLE_CLR, 1);
	else
		omap_i2c_write_reg(dev, OMAP_I2C_IE_REG, 0);

	if (dev->rev < OMAP_I2C_REV_2) {
		iv = omap_i2c_read_reg(dev, OMAP_I2C_IV_REG); /* Read clears */
	} else {
		omap_i2c_write_reg(dev, OMAP_I2C_STAT_REG, dev->iestate);

		/* Flush posted write before the dev->idle store occurs */
		omap_i2c_read_reg(dev, OMAP_I2C_STAT_REG);
	}
	dev->idle = 1;

	pm_runtime_put_sync(&pdev->dev);
}

static int omap_i2c_init(struct omap_i2c_dev *dev)
{
	u16 psc = 0, scll = 0, sclh = 0, buf = 0;
	u16 fsscll = 0, fssclh = 0, hsscll = 0, hssclh = 0;
	unsigned long fclk_rate = 12000000;
	unsigned long timeout;
	unsigned long internal_clk = 0;
	struct clk *fclk;

	if (dev->rev >= OMAP_I2C_REV_2) {
		/* Disable I2C controller before soft reset */
		omap_i2c_write_reg(dev, OMAP_I2C_CON_REG,
			omap_i2c_read_reg(dev, OMAP_I2C_CON_REG) &
				~(OMAP_I2C_CON_EN));

		omap_i2c_write_reg(dev, OMAP_I2C_SYSC_REG, SYSC_SOFTRESET_MASK);
		/* For some reason we need to set the EN bit before the
		 * reset done bit gets set. */
		timeout = jiffies + OMAP_I2C_TIMEOUT;
		omap_i2c_write_reg(dev, OMAP_I2C_CON_REG, OMAP_I2C_CON_EN);
		while (!(omap_i2c_read_reg(dev, OMAP_I2C_SYSS_REG) &
			 SYSS_RESETDONE_MASK)) {
			if (time_after(jiffies, timeout)) {
				dev_warn(dev->dev, "timeout waiting "
						"for controller reset\n");
				return -ETIMEDOUT;
			}
			msleep(1);
		}

		/* SYSC register is cleared by the reset; rewrite it */
		if (dev->rev == OMAP_I2C_REV_ON_2430) {

			omap_i2c_write_reg(dev, OMAP_I2C_SYSC_REG,
					   SYSC_AUTOIDLE_MASK);

		} else if (dev->rev >= OMAP_I2C_REV_ON_3430) {
			dev->syscstate = SYSC_AUTOIDLE_MASK;
			dev->syscstate |= SYSC_ENAWAKEUP_MASK;
			dev->syscstate |= (SYSC_IDLEMODE_SMART <<
			      __ffs(SYSC_SIDLEMODE_MASK));
			dev->syscstate |= (SYSC_CLOCKACTIVITY_FCLK <<
			      __ffs(SYSC_CLOCKACTIVITY_MASK));

			omap_i2c_write_reg(dev, OMAP_I2C_SYSC_REG,
							dev->syscstate);
			/*
			 * Enabling all wakup sources to stop I2C freezing on
			 * WFI instruction.
			 * REVISIT: Some wkup sources might not be needed.
			 */
			dev->westate = OMAP_I2C_WE_ALL;
			if (dev->rev < OMAP_I2C_REV_ON_4430)
				omap_i2c_write_reg(dev, OMAP_I2C_WE_REG,
								dev->westate);
		}
	}
	omap_i2c_write_reg(dev, OMAP_I2C_CON_REG, 0);

	if (cpu_class_is_omap1()) {
		/*
		 * The I2C functional clock is the armxor_ck, so there's
		 * no need to get "armxor_ck" separately.  Now, if OMAP2420
		 * always returns 12MHz for the functional clock, we can
		 * do this bit unconditionally.
		 */
		fclk = clk_get(dev->dev, "fck");
		fclk_rate = clk_get_rate(fclk);
		clk_put(fclk);

		/* TRM for 5912 says the I2C clock must be prescaled to be
		 * between 7 - 12 MHz. The XOR input clock is typically
		 * 12, 13 or 19.2 MHz. So we should have code that produces:
		 *
		 * XOR MHz	Divider		Prescaler
		 * 12		1		0
		 * 13		2		1
		 * 19.2		2		1
		 */
		if (fclk_rate > 12000000)
			psc = fclk_rate / 12000000;
	}

	if (!(cpu_class_is_omap1() || cpu_is_omap2420())) {

		/*
		 * HSI2C controller internal clk rate should be 19.2 Mhz for
		 * HS and for all modes on 2430. On 34xx we can use lower rate
		 * to get longer filter period for better noise suppression.
		 * The filter is iclk (fclk for HS) period.
		 */
		if (dev->speed > 400 || cpu_is_omap2430())
			internal_clk = 19200;
		else if (dev->speed > 100)
			internal_clk = 9600;
		else
			internal_clk = 4000;
		fclk = clk_get(dev->dev, "fck");
		fclk_rate = clk_get_rate(fclk) / 1000;
		clk_put(fclk);

		/* Compute prescaler divisor */
		psc = fclk_rate / internal_clk;
		psc = psc - 1;

		/* If configured for High Speed */
		if (dev->speed > 400) {
			unsigned long scl;

			/* For first phase of HS mode */
			scl = internal_clk / 400;
			fsscll = scl - (scl / 3) - 7;
			fssclh = (scl / 3) - 5;

			/* For second phase of HS mode */
			scl = fclk_rate / dev->speed;
			hsscll = scl - (scl / 3) - 7;
			hssclh = (scl / 3) - 5;
		} else if (dev->speed > 100) {
			unsigned long scl;

			/* Fast mode */
			scl = internal_clk / dev->speed;
			fsscll = scl - (scl / 3) - 7;
			fssclh = (scl / 3) - 5;
		} else {
			/* Standard mode */
			fsscll = internal_clk / (dev->speed * 2) - 7;
			fssclh = internal_clk / (dev->speed * 2) - 5;
		}
		scll = (hsscll << OMAP_I2C_SCLL_HSSCLL) | fsscll;
		sclh = (hssclh << OMAP_I2C_SCLH_HSSCLH) | fssclh;
	} else {
		/* Program desired operating rate */
		fclk_rate /= (psc + 1) * 1000;
		if (psc > 2)
			psc = 2;
		scll = fclk_rate / (dev->speed * 2) - 7 + psc;
		sclh = fclk_rate / (dev->speed * 2) - 7 + psc;
	}

	/* Setup clock prescaler to obtain approx 12MHz I2C module clock: */
	omap_i2c_write_reg(dev, OMAP_I2C_PSC_REG, psc);

	/* SCL low and high time values */
	omap_i2c_write_reg(dev, OMAP_I2C_SCLL_REG, scll);
	omap_i2c_write_reg(dev, OMAP_I2C_SCLH_REG, sclh);

	if (dev->fifo_size) {
		/* Note: setup required fifo size - 1. RTRSH and XTRSH */
		buf = (dev->fifo_size - 1) << 8 | OMAP_I2C_BUF_RXFIF_CLR |
			(dev->fifo_size - 1) | OMAP_I2C_BUF_TXFIF_CLR;
		omap_i2c_write_reg(dev, OMAP_I2C_BUF_REG, buf);
	}

	/* Take the I2C module out of reset: */
	omap_i2c_write_reg(dev, OMAP_I2C_CON_REG, OMAP_I2C_CON_EN);

	dev->errata = 0;

	if (cpu_is_omap2430() || cpu_is_omap34xx())
		dev->errata |= I2C_OMAP_ERRATA_I207;

	/* Enable interrupts */
	dev->iestate = (OMAP_I2C_IE_XRDY | OMAP_I2C_IE_RRDY |
			OMAP_I2C_IE_ARDY | OMAP_I2C_IE_NACK |
			OMAP_I2C_IE_AL)  | ((dev->fifo_size) ?
				(OMAP_I2C_IE_RDR | OMAP_I2C_IE_XDR) : 0);
	omap_i2c_write_reg(dev, OMAP_I2C_IE_REG, dev->iestate);
	if (cpu_is_omap34xx()) {
		dev->pscstate = psc;
		dev->scllstate = scll;
		dev->sclhstate = sclh;
		dev->bufstate = buf;
	}
	return 0;
}

/*
 * Waiting on Bus Busy
 */
static int omap_i2c_wait_for_bb(struct omap_i2c_dev *dev)
{
	unsigned long timeout;

	timeout = jiffies + OMAP_I2C_TIMEOUT;
	while (omap_i2c_read_reg(dev, OMAP_I2C_STAT_REG) & OMAP_I2C_STAT_BB) {
		if (time_after(jiffies, timeout)) {
			dev_warn(dev->dev, "timeout waiting for bus ready\n");
			return -ETIMEDOUT;
		}
		msleep(1);
	}

	return 0;
}

/*
 * Low level master read/write transaction.
 */
static int omap_i2c_xfer_msg(struct i2c_adapter *adap,
			     struct i2c_msg *msg, int stop)
{
	struct omap_i2c_dev *dev = i2c_get_adapdata(adap);
	int r;
	u16 w;

	dev_dbg(dev->dev, "addr: 0x%04x, len: %d, flags: 0x%x, stop: %d\n",
		msg->addr, msg->len, msg->flags, stop);
	printk("[%s]addr: 0x%04x, len: %d, flags: 0x%x, stop: %d\n",
		__func__, msg->addr, msg->len, msg->flags, stop);


	if (msg->len == 0)
		return -EINVAL;


	omap_i2c_write_reg(dev, OMAP_I2C_SA_REG, msg->addr);

	/* REVISIT: Could the STB bit of I2C_CON be used with probing? */
	dev->buf = msg->buf;
	dev->buf_len = msg->len;

	omap_i2c_write_reg(dev, OMAP_I2C_CNT_REG, dev->buf_len);

	/* Clear the FIFO Buffers */
	w = omap_i2c_read_reg(dev, OMAP_I2C_BUF_REG);
	w |= OMAP_I2C_BUF_RXFIF_CLR | OMAP_I2C_BUF_TXFIF_CLR;
	omap_i2c_write_reg(dev, OMAP_I2C_BUF_REG, w);

	init_completion(&dev->cmd_complete);
	dev->cmd_err = 0;

	w = OMAP_I2C_CON_EN | OMAP_I2C_CON_MST | OMAP_I2C_CON_STT;

	/* High speed configuration */
	if (dev->speed > 400)
		w |= OMAP_I2C_CON_OPMODE_HS;

	if (msg->flags & I2C_M_TEN)
		w |= OMAP_I2C_CON_XA;
	if (!(msg->flags & I2C_M_RD))
		w |= OMAP_I2C_CON_TRX;

	if (!dev->b_hw && stop)
		w |= OMAP_I2C_CON_STP;

	omap_i2c_write_reg(dev, OMAP_I2C_CON_REG, w);

	/*
	 * Don't write stt and stp together on some hardware.
	 */
	if (dev->b_hw && stop) {
		unsigned long delay = jiffies + OMAP_I2C_TIMEOUT;
		u16 con = omap_i2c_read_reg(dev, OMAP_I2C_CON_REG);
		while (con & OMAP_I2C_CON_STT) {
			con = omap_i2c_read_reg(dev, OMAP_I2C_CON_REG);

			/* Let the user know if i2c is in a bad state */
			if (time_after(jiffies, delay)) {
				dev_err(dev->dev, "controller timed out "
				"waiting for start condition to finish\n");
				return -ETIMEDOUT;
			}
			cpu_relax();
		}

		w |= OMAP_I2C_CON_STP;
		w &= ~OMAP_I2C_CON_STT;
		omap_i2c_write_reg(dev, OMAP_I2C_CON_REG, w);
	}

	/*
	 * REVISIT: We should abort the transfer on signals, but the bus goes
	 * into arbitration and we're currently unable to recover from it.
	 */
	if (dev->set_mpu_wkup_lat != NULL)
		dev->set_mpu_wkup_lat(dev->dev, dev->latency);
	r = wait_for_completion_timeout(&dev->cmd_complete,
					OMAP_I2C_TIMEOUT);
	if (dev->set_mpu_wkup_lat != NULL)
		dev->set_mpu_wkup_lat(dev->dev, -1);
	dev->buf_len = 0;

	printk("[%s]leave r:0x%x\n", r);
	if (r < 0)
		return r;
	if (r == 0) {
		dev_err(dev->dev, "controller timed out\n");
		omap_i2c_init(dev);
		return -ETIMEDOUT;
	}

	if (likely(!dev->cmd_err))
		return 0;

	/* We have an error */
	if (dev->cmd_err & (OMAP_I2C_STAT_AL | OMAP_I2C_STAT_ROVR |
			    OMAP_I2C_STAT_XUDF)) {
		omap_i2c_init(dev);
		return -EIO;
	}

	if (dev->cmd_err & OMAP_I2C_STAT_NACK) {
		return -EREMOTEIO;
	}
	return -EIO;
}


/*
 * Prepare controller for a transaction and call omap_i2c_xfer_msg
 * to do the work during IRQ processing.
 */
static int
omap_i2c_xfer(struct i2c_adapter *adap, struct i2c_msg msgs[], int num)
{
	struct omap_i2c_dev *dev = i2c_get_adapdata(adap);
	int i;
	int r;

	omap_i2c_unidle(dev);

	r = omap_i2c_wait_for_bb(dev);
	if (r < 0)
		goto out;

	for (i = 0; i < num; i++) {
		r = omap_i2c_xfer_msg(adap, &msgs[i], (i == (num - 1)));
		if (r != 0)
			break;
	}

	if (r == 0)
		r = num;

	omap_i2c_wait_for_bb(dev);
out:
	omap_i2c_idle(dev);
	return r;
}

static u32
omap_i2c_func(struct i2c_adapter *adap)
{
	return I2C_FUNC_I2C | (I2C_FUNC_SMBUS_EMUL & ~I2C_FUNC_SMBUS_QUICK);
}

static inline void
omap_i2c_complete_cmd(struct omap_i2c_dev *dev, u16 err)
{
	dev->cmd_err |= err;
	complete(&dev->cmd_complete);
}

static inline void
omap_i2c_ack_stat(struct omap_i2c_dev *dev, u16 stat)
{
	omap_i2c_write_reg(dev, OMAP_I2C_STAT_REG, stat);
}

static inline void i2c_omap_errata_i207(struct omap_i2c_dev *dev, u16 stat)
{
	/*
	 * I2C Errata(Errata Nos. OMAP2: 1.67, OMAP3: 1.8)
	 * Not applicable for OMAP4.
	 * Under certain rare conditions, RDR could be set again
	 * when the bus is busy, then ignore the interrupt and
	 * clear the interrupt.
	 */
	if (stat & OMAP_I2C_STAT_RDR) {
		/* Step 1: If RDR is set, clear it */
		omap_i2c_ack_stat(dev, OMAP_I2C_STAT_RDR);

		/* Step 2: */
		if (!(omap_i2c_read_reg(dev, OMAP_I2C_STAT_REG)
						& OMAP_I2C_STAT_BB)) {

			/* Step 3: */
			if (omap_i2c_read_reg(dev, OMAP_I2C_STAT_REG)
						& OMAP_I2C_STAT_RDR) {
				omap_i2c_ack_stat(dev, OMAP_I2C_STAT_RDR);
				dev_dbg(dev->dev, "RDR when bus is busy.\n");
			}

		}
	}
}

/* rev1 devices are apparently only on some 15xx */
#ifdef CONFIG_ARCH_OMAP15XX

static irqreturn_t
omap_i2c_rev1_isr(int this_irq, void *dev_id)
{
	struct omap_i2c_dev *dev = dev_id;
	u16 iv, w;

	if (dev->idle)
		return IRQ_NONE;

	iv = omap_i2c_read_reg(dev, OMAP_I2C_IV_REG);
	switch (iv) {
	case 0x00:	/* None */
		break;
	case 0x01:	/* Arbitration lost */
		dev_err(dev->dev, "[omap_i2c_rev1_isr] Arbitration lost\n");
		omap_i2c_complete_cmd(dev, OMAP_I2C_STAT_AL);
		break;
	case 0x02:	/* No acknowledgement */
		omap_i2c_complete_cmd(dev, OMAP_I2C_STAT_NACK);
		omap_i2c_write_reg(dev, OMAP_I2C_CON_REG, OMAP_I2C_CON_STP);
		break;
	case 0x03:	/* Register access ready */
		omap_i2c_complete_cmd(dev, 0);
		break;
	case 0x04:	/* Receive data ready */
		if (dev->buf_len) {
			w = omap_i2c_read_reg(dev, OMAP_I2C_DATA_REG);
			*dev->buf++ = w;
			dev->buf_len--;
			if (dev->buf_len) {
				*dev->buf++ = w >> 8;
				dev->buf_len--;
			}
		} else
			dev_err(dev->dev, "RRDY IRQ while no data requested\n");
		break;
	case 0x05:	/* Transmit data ready */
		if (dev->buf_len) {
			w = *dev->buf++;
			dev->buf_len--;
			if (dev->buf_len) {
				w |= *dev->buf++ << 8;
				dev->buf_len--;
			}
			omap_i2c_write_reg(dev, OMAP_I2C_DATA_REG, w);
		} else
			dev_err(dev->dev, "XRDY IRQ while no data to send\n");
		break;
	default:
		return IRQ_NONE;
	}

	return IRQ_HANDLED;
}
#else
#define omap_i2c_rev1_isr		NULL
#endif

/*
 * OMAP3430 Errata 1.153: When an XRDY/XDR is hit, wait for XUDF before writing
 * data to DATA_REG. Otherwise some data bytes can be lost while transferring
 * them from the memory to the I2C interface.
 */
static int errata_omap3_1p153(struct omap_i2c_dev *dev, u16 *stat, int *err)
{
	unsigned long timeout = 10000;

	while (--timeout && !(*stat & OMAP_I2C_STAT_XUDF)) {
		if (*stat & (OMAP_I2C_STAT_NACK | OMAP_I2C_STAT_AL)) {
			omap_i2c_ack_stat(dev, *stat & (OMAP_I2C_STAT_XRDY |
							OMAP_I2C_STAT_XDR));
			*err |= OMAP_I2C_STAT_XUDF;
			return -ETIMEDOUT;
		}

		cpu_relax();
		*stat = omap_i2c_read_reg(dev, OMAP_I2C_STAT_REG);
	}

	if (!timeout) {
		dev_err(dev->dev, "timeout waiting on XUDF bit\n");
		return 0;
	}

	return 0;
}

static irqreturn_t
omap_i2c_isr(int this_irq, void *dev_id)
{
	struct omap_i2c_dev *dev = dev_id;
	u16 bits;
	u16 stat, w;
	int err, count = 0;
	// kisung cho
	u16 addr;

	if (dev->idle)
		return IRQ_NONE;
	printk("[%s]enter\n", __func__);
	addr = omap_i2c_read_reg(dev, OMAP_I2C_SA_REG);

	bits = omap_i2c_read_reg(dev, OMAP_I2C_IE_REG);
	while ((stat = (omap_i2c_read_reg(dev, OMAP_I2C_STAT_REG))) & bits) {
		dev_dbg(dev->dev, "IRQ (ISR = 0x%04x)\n", stat);
		if (count++ == 100) {
			dev_warn(dev->dev, "Too much work in one IRQ\n");
			break;
		}
		printk( "[%s]IRQ (ISR = 0x%04x), addr:0x%x\n", __func__, stat, addr);
		if(stat & OMAP_I2C_STAT_ARDY ){
			printk( "\tOMAP_I2C_STAT_ARDY\n", __func__);
		}
		if(stat & OMAP_I2C_STAT_RRDY ){
			printk( "\tOMAP_I2C_STAT_RRDY\n", __func__);
		}
		if(stat & OMAP_I2C_STAT_RDR ){
			printk( "\tOMAP_I2C_STAT_RDR\n", __func__);
		}
		if(stat & OMAP_I2C_STAT_XRDY ){
			printk( "\tOMAP_I2C_STAT_XRDY\n", __func__);
		}
		if(stat & OMAP_I2C_STAT_AL ){
			printk( "\tOMAP_I2C_STAT_AL\n", __func__);
		}
		if(stat & OMAP_I2C_STAT_NACK ){
			printk( "\tOMAP_I2C_STAT_NACK\n", __func__);
		}

		err = 0;
complete:
		/*
		 * Ack the stat in one go, but [R/X]DR and [R/X]RDY should be
		 * acked after the data operation is complete.
		 * Ref: TRM SWPU114Q Figure 18-31
		 */
		omap_i2c_write_reg(dev, OMAP_I2C_STAT_REG, stat &
				~(OMAP_I2C_STAT_RRDY | OMAP_I2C_STAT_RDR |
				OMAP_I2C_STAT_XRDY | OMAP_I2C_STAT_XDR));
		
		if (stat & OMAP_I2C_STAT_NACK) {
			err |= OMAP_I2C_STAT_NACK;
			omap_i2c_write_reg(dev, OMAP_I2C_CON_REG,
				omap_i2c_read_reg(dev, OMAP_I2C_CON_REG) | OMAP_I2C_CON_STP);
			printk("[%s]OMAP_I2C_CON_STP\n", __func__);
		}
		if (stat & OMAP_I2C_STAT_AL) {
			dev_err(dev->dev, "[omap_i2c_isr] Arbitration lost\n");
			err |= OMAP_I2C_STAT_AL;
			if(addr == 0x52){
				 omap_i2c_ack_stat(dev, OMAP_I2C_STAT_AL);
			}
		}
		if (stat & (OMAP_I2C_STAT_ARDY | OMAP_I2C_STAT_NACK | OMAP_I2C_STAT_AL)) {
			omap_i2c_ack_stat(dev, stat &
				(OMAP_I2C_STAT_RRDY | OMAP_I2C_STAT_RDR |
				OMAP_I2C_STAT_XRDY | OMAP_I2C_STAT_XDR));
			omap_i2c_write_reg(dev, OMAP_I2C_BUF_REG,
				omap_i2c_read_reg(dev, OMAP_I2C_BUF_REG) |
				OMAP_I2C_BUF_RXFIF_CLR |
				OMAP_I2C_BUF_TXFIF_CLR);
			omap_i2c_complete_cmd(dev, err);
			printk("[%s]IRQ_HANDLED\n", __func__);
			return IRQ_HANDLED;
		}
		if (stat & (OMAP_I2C_STAT_RRDY | OMAP_I2C_STAT_RDR)) {
			u8 num_bytes = 1;
			//printk("OMAP_I2C_STAT_RRDY | OMAP_I2C_STAT_RDR\n");
			if (dev->errata & I2C_OMAP_ERRATA_I207)
				i2c_omap_errata_i207(dev, stat);

			if (dev->fifo_size) {
				if (stat & OMAP_I2C_STAT_RRDY)
					num_bytes = dev->fifo_size;
				else    /* read RXSTAT on RDR interrupt */
					num_bytes = (omap_i2c_read_reg(dev,
							OMAP_I2C_BUFSTAT_REG)
							>> 8) & 0x3F;
			}
			if(addr == 0x52){
				num_bytes = 1;
			}

			while (num_bytes) {
				num_bytes--;
				w = omap_i2c_read_reg(dev, OMAP_I2C_DATA_REG);
				printk("[%d]buf_len:%d\n", __LINE__, dev->buf_len);
				if (dev->buf_len) {
					*dev->buf++ = w;
					dev->buf_len--;
					/*
					 * Data reg in 2430, omap3 and
					 * omap4 is 8 bit wide
					 */
					if (cpu_class_is_omap1() ||
							cpu_is_omap2420()) {
						if (dev->buf_len) {
							*dev->buf++ = w >> 8;
							dev->buf_len--;
						}
					}
				} else {
					if (stat & OMAP_I2C_STAT_RRDY)
						dev_err(dev->dev,
							"RRDY IRQ while no data"
								" requested\n");
					if (stat & OMAP_I2C_STAT_RDR)
						dev_err(dev->dev,
							"RDR IRQ while no data"
								" requested\n");
					break;
				}
			}
			omap_i2c_ack_stat(dev, stat & (OMAP_I2C_STAT_RRDY | OMAP_I2C_STAT_RDR));
			continue;
		}
		if (stat & (OMAP_I2C_STAT_XRDY | OMAP_I2C_STAT_XDR)) {
			u8 num_bytes = 1;
			printk("OMAP_I2C_STAT_XRDY | OMAP_I2C_STAT_XDR\n");
			if (dev->fifo_size) {
				if (stat & OMAP_I2C_STAT_XRDY)
					num_bytes = dev->fifo_size;
				else    /* read TXSTAT on XDR interrupt */
					num_bytes = omap_i2c_read_reg(dev,
							OMAP_I2C_BUFSTAT_REG)
							& 0x3F;
			}
			while (num_bytes) {
				num_bytes--;
				w = 0;
				if (dev->buf_len) {
					w = *dev->buf++;
					dev->buf_len--;
					/*
					 * Data reg in 2430, omap3 and
					 * omap4 is 8 bit wide
					 */
					if (cpu_class_is_omap1() ||
							cpu_is_omap2420()) {
						if (dev->buf_len) {
							w |= *dev->buf++ << 8;
							dev->buf_len--;
						}
					}
				} else {
					if (stat & OMAP_I2C_STAT_XRDY)
						dev_err(dev->dev,
							"XRDY IRQ while no "
							"data to send\n");
					if (stat & OMAP_I2C_STAT_XDR)
						dev_err(dev->dev,
							"XDR IRQ while no "
							"data to send\n");
					break;
				}

				if ((dev->errata & I2C_OMAP3_1P153) &&
				    errata_omap3_1p153(dev, &stat, &err))
					goto complete;

				omap_i2c_write_reg(dev, OMAP_I2C_DATA_REG, w);
			}
			omap_i2c_ack_stat(dev, stat & (OMAP_I2C_STAT_XRDY | OMAP_I2C_STAT_XDR));
#if 0
			// kisung cho
			if(addr == 0x52){
				omap_i2c_write_reg(dev, OMAP_I2C_STAT_REG, stat &
					~(OMAP_I2C_STAT_RRDY | OMAP_I2C_STAT_RDR |
					OMAP_I2C_STAT_XRDY | OMAP_I2C_STAT_XDR));
	
				w = omap_i2c_read_reg(dev, OMAP_I2C_DATA_REG);
				printk("[%s]first i2c_data_reg:0x%x buf_len:%d\n", __func__, w, dev->buf_len);
				omap_i2c_ack_stat(dev, stat & (OMAP_I2C_STAT_RRDY | OMAP_I2C_STAT_RDR));
				w = omap_i2c_read_reg(dev, OMAP_I2C_DATA_REG);
				printk("[%s]second i2c_data_reg:0x%x buf_len:%d\n", __func__, w, dev->buf_len);
				omap_i2c_ack_stat(dev, stat & (OMAP_I2C_STAT_RRDY | OMAP_I2C_STAT_RDR));
				
			}
			// end
#endif
			continue;
		}
		if (stat & OMAP_I2C_STAT_ROVR) {
			dev_err(dev->dev, "Receive overrun\n");
			dev->cmd_err |= OMAP_I2C_STAT_ROVR;
		}
		if (stat & OMAP_I2C_STAT_XUDF) {
			dev_err(dev->dev, "Transmit underflow\n");
			dev->cmd_err |= OMAP_I2C_STAT_XUDF;
		}
	}
	printk("[%s]leave\n", __func__);
	return count ? IRQ_HANDLED : IRQ_NONE;
}

static const struct i2c_algorithm omap_i2c_algo = {
	.master_xfer	= omap_i2c_xfer,
	.functionality	= omap_i2c_func,
};

static int __devinit
omap_i2c_probe(struct platform_device *pdev)
{
	struct omap_i2c_dev	*dev;
	struct i2c_adapter	*adap;
	struct resource		*mem, *irq, *ioarea;
	struct omap_i2c_bus_platform_data *pdata = pdev->dev.platform_data;
	irq_handler_t isr;
	int r;
	u32 speed = 0;

	/* NOTE: driver uses the static register mapping */
	mem = platform_get_resource(pdev, IORESOURCE_MEM, 0);
	if (!mem) {
		dev_err(&pdev->dev, "no mem resource?\n");
		return -ENODEV;
	}
	irq = platform_get_resource(pdev, IORESOURCE_IRQ, 0);
	if (!irq) {
		dev_err(&pdev->dev, "no irq resource?\n");
		return -ENODEV;
	}

	ioarea = request_mem_region(mem->start, resource_size(mem),
			pdev->name);
	if (!ioarea) {
		dev_err(&pdev->dev, "I2C region already claimed\n");
		return -EBUSY;
	}

	dev = kzalloc(sizeof(struct omap_i2c_dev), GFP_KERNEL);
	if (!dev) {
		r = -ENOMEM;
		goto err_release_region;
	}

	if (pdata != NULL) {
		speed = pdata->clkrate;
		dev->set_mpu_wkup_lat = pdata->set_mpu_wkup_lat;
	} else {
		speed = 100;	/* Default speed */
		dev->set_mpu_wkup_lat = NULL;
	}

	dev->speed = speed;
	dev->idle = 1;
	dev->dev = &pdev->dev;
	dev->irq = irq->start;
	dev->base = ioremap(mem->start, resource_size(mem));
	if (!dev->base) {
		r = -ENOMEM;
		goto err_free_mem;
	}

	platform_set_drvdata(pdev, dev);

	if (cpu_is_omap7xx())
		dev->reg_shift = 1;
	else if (cpu_is_omap44xx() || cpu_is_ti81xx())
		dev->reg_shift = 0;
	else
		dev->reg_shift = 2;

	if (cpu_is_omap44xx() || cpu_is_ti81xx())
		dev->regs = (u8 *) omap4_reg_map;
	else
		dev->regs = (u8 *) reg_map;

	pm_runtime_enable(&pdev->dev);
	omap_i2c_unidle(dev);

	dev->rev = omap_i2c_read_reg(dev, OMAP_I2C_REV_REG) & 0xff;

	if (dev->rev <= OMAP_I2C_REV_ON_3430)
		dev->errata |= I2C_OMAP3_1P153;

	if (!(cpu_class_is_omap1() || cpu_is_omap2420())) {
		u16 s;

		/* Set up the fifo size - Get total size */
		s = (omap_i2c_read_reg(dev, OMAP_I2C_BUFSTAT_REG) >> 14) & 0x3;
		dev->fifo_size = 0x8 << s;

		/*
		 * Set up notification threshold as half the total available
		 * size. This is to ensure that we can handle the status on int
		 * call back latencies.
		 */
		if (dev->rev >= OMAP_I2C_REV_ON_4430) {
			dev->fifo_size = 0;
			dev->b_hw = 0; /* Disable hardware fixes */
		} else {
			dev->fifo_size = (dev->fifo_size / 2);
			dev->b_hw = 1; /* Enable hardware fixes */
		}
		/* calculate wakeup latency constraint for MPU */
		if (dev->set_mpu_wkup_lat != NULL)
			dev->latency = (1000000 * dev->fifo_size) /
				       (1000 * speed / 8);
	}

	/* reset ASAP, clearing any IRQs */
	omap_i2c_init(dev);

	isr = (dev->rev < OMAP_I2C_REV_2) ? omap_i2c_rev1_isr : omap_i2c_isr;
	r = request_irq(dev->irq, isr, 0, pdev->name, dev);

	if (r) {
		dev_err(dev->dev, "failure requesting irq %i\n", dev->irq);
		goto err_unuse_clocks;
	}

	dev_info(dev->dev, "bus %d rev%d.%d at %d kHz\n",
		 pdev->id, dev->rev >> 4, dev->rev & 0xf, dev->speed);

	omap_i2c_idle(dev);

	adap = &dev->adapter;
	i2c_set_adapdata(adap, dev);
	adap->owner = THIS_MODULE;
	adap->class = I2C_CLASS_HWMON;
	strlcpy(adap->name, "OMAP I2C adapter", sizeof(adap->name));
	adap->algo = &omap_i2c_algo;
	adap->dev.parent = &pdev->dev;

	/* i2c device drivers may be active on return from add_adapter() */
	adap->nr = pdev->id;
	r = i2c_add_numbered_adapter(adap);
	if (r) {
		dev_err(dev->dev, "failure adding adapter\n");
		goto err_free_irq;
	}

	return 0;

err_free_irq:
	free_irq(dev->irq, dev);
err_unuse_clocks:
	omap_i2c_write_reg(dev, OMAP_I2C_CON_REG, 0);
	omap_i2c_idle(dev);
	iounmap(dev->base);
err_free_mem:
	platform_set_drvdata(pdev, NULL);
	kfree(dev);
err_release_region:
	release_mem_region(mem->start, resource_size(mem));

	return r;
}

static int
omap_i2c_remove(struct platform_device *pdev)
{
	struct omap_i2c_dev	*dev = platform_get_drvdata(pdev);
	struct resource		*mem;

	platform_set_drvdata(pdev, NULL);

	free_irq(dev->irq, dev);
	i2c_del_adapter(&dev->adapter);
	omap_i2c_write_reg(dev, OMAP_I2C_CON_REG, 0);
	iounmap(dev->base);
	kfree(dev);
	mem = platform_get_resource(pdev, IORESOURCE_MEM, 0);
	release_mem_region(mem->start, resource_size(mem));
	return 0;
}

static struct platform_driver omap_i2c_driver = {
	.probe		= omap_i2c_probe,
	.remove		= omap_i2c_remove,
	.driver		= {
		.name	= "omap_i2c",
		.owner	= THIS_MODULE,
	},
};

/* I2C may be needed to bring up other drivers */
static int __init
omap_i2c_init_driver(void)
{
	return platform_driver_register(&omap_i2c_driver);
}
subsys_initcall(omap_i2c_init_driver);

static void __exit omap_i2c_exit_driver(void)
{
	platform_driver_unregister(&omap_i2c_driver);
}
module_exit(omap_i2c_exit_driver);

MODULE_AUTHOR("MontaVista Software, Inc. (and others)");
MODULE_DESCRIPTION("TI OMAP I2C bus adapter");
MODULE_LICENSE("GPL");
MODULE_ALIAS("platform:omap_i2c");
  and it sequeuce is write read addr -> ack -> read 8bit data -> ack -> read 8bit data-> ack

but it always occured Aribitration error.

how can i fix this issue?

any advice will be appreciated.

Thanks.