I are using the demo of DM368 borad to encode HD video in H264 from TVP7002.
when 720P@60P is used on input and run the demo, the framerate aways is 22fps. For the frameate is 30 fps, I should HOW to set the parameters ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
What codebase are you using? is it based on DVSDK?
Can you check with IPNC RDK codebase, we have 720p60 usecase on DM368
Please ensure you have the latest codecs which supports the HIGH SPEED encoding preset
Latest codec version is 2.30.00.06
Are you also observing drop on capture side as well? can you check your capture rate by turning OFF encoding, are you observing 60fps with capture only?
Also, please check if your UBL has all the changes for DM368 clocks
Regards,
Raghu
Hello,
Please contact local TI sales or FAE to get this.
If you have IPNC RDK, you can pick from this
Regards,
Raghu