Hello,
In the 6636 Datasheet, it says 2x TCP2 and supports 282 Mbps for LTE. In the 6638 Datasheet it says 4x TCP2 and supports 282 Mbps for LTE. Does it mean these values are per Coprocessor or is it total throughput over all of the TCP Coprocessors. Same notation is used for VCP2 and FFTC too.
Do I have to simply multiply the data rate by the number of the coprocessors for the total throughput?
Thanks.