Other Parts Discussed in Thread: TMS320C6678, SYSBIOS
Hi everybody,
I'm new to TMS320C6678 and I want to ask you if is possible to run two C function totally in parallel on different cores with this kind of DSP .
To be clear:
if I have an array of 1024 elements, and want to do a sum of all this element (just to give an example), can I write 2 separate C function that do the sum of the first 512 element and the sum of the least 512 element, running totally in parallel in 2 different cores?
like: uint32_t sum1(..,..) running on core 0 and uint32_t sum2(...,...) running on core1?
If it's possible can someone link me the documentation with which I can learn this kind of things?
thank you in advance
Carmine