HI..
now days I'm testing my ICE board as etherCAT slave..
so I just add some index for ethercat Object Dictionary.. and I maped that object to PDO (0x1602)
I thought it works properly... but there is Lost Frame error in OP mode (ethercat state machine)
so i'm trying to find out what is problem...
and I found EtherCAT example from TI has no Lost Frame.. so I just changed size of existing index(0x7020 Motor output count & cmd) 8 bit -> UINT16
and now I can still see Lost Frame on Twincat 2
what is problem ?? ind_sdk_1.0.0.5 has problem??
Or is this bug of PRU firmware ??
please help me.. below is my capture file..
thanks in advance..
Moonseon