Hi All,
I'm using the image processing program IPC-Based project will run on a c6670 EVM.
Demo program runs correctly. But when I build the project IPC and make the “master.out”file, with the loaded application on core 0 (Master Core), ccs program closes and when I build the “slave.out” file, with the loaded application on core # (slave core: 1,2,3) I see an error:
C66xx_1: GEL Output: Setup_Memory_Map...
C66xx_1: GEL Output: Setup_Memory_Map... Done.
C66xx_1: GEL Output: Setup Cache...
C66xx_1: GEL Output: L1P = 32K
C66xx_1: GEL Output: L1D = 32K
C66xx_1: GEL Output: L2 = ALL SRAM
C66xx_1: GEL Output: Setup Cache... Done.
C66xx_1: GEL Output: Invalidate All Cache...
C66xx_1: GEL Output: Invalidate All Cache... Done.
C66xx_1: GEL Output: GEL Reset...
C66xx_1: GEL Output: GEL Reset... Done.
C66xx_1: Trouble Writing Register PC: (Error -1176 @ 0x0) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.73.0)
C66xx_1: Symbol Manager: the object file contains multiple sets of debug information; only the first set will be used.
How do I edit this demo project and I use this program?
Ccs v5.4:
Ipc 1.25.3.15
Mcsdk 1.1.2.6
Ndk 2.22.3.20
Sys/bios 6.35.3.47
Uia 1.3.1.08
Thank you for your reply