Dear all,
I am working on DVSDK version 2.10.01.18. My issue:
DM368 decoder can receive the encoded frame 720p high profile directly via UDP protocol from network.
+ If I save those encoded frame into a file, then I use VLC player to play the file and it works well. But when I decode those encoded frame and display by using the dvsdk_2_10_01_18/dvsdk_demos_2_10_00_17/dm365/decode/video.c. Decoder decodes and displays some the first frames and then it was blocked at fifoRet = Fifo_get(envp->hDisplayOutFifo, &hDispBuf) function at line 410 in main loop as file attached:6786.video.c
+ Analysis the file which I saved like this:
Any one help me! Thank you very much!