Hi,
we do have some problems with the initialisation of control registers in the McASP..
The initialization attempt of the control registers for the McASP-
Function blocks does not work.
The initialization of the other control registers
does work: The EMIF register (External Memory
Interface), I can adapt to the available memory type and PINMUX register (from the group and the System Configuration tab SYSCFG0) can also describe in their own values, so that the McBSP function blocks are connected to the DSP pins.
What may we do ?