This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Query regarding standalone H.264 decoder for DaVinci....

Hi,

I want to know is there's any standalone implementation available for DM6437 DaVinci board for the H.264 decoder. With the original demo pack, only encoder/decoder parts working sequentially on each frame are available.

I also want to know if those codes can be modified to create a decoder, that takes a separate file and decodes it. As the logic in those codes is such that, the decoder uses some arguments passed down by the encode part at that very time, WHICH I GUESS WON'T BE AVAILABLE IF YOU ARE READING FROM A SEPARATE FILE.

Thanks!                    JUST SUGGESTION IF POSSIBLE, REQUIRED, KINDLY HELP....